2022-02-12 12:18 AM - edited 2023-11-20 8:36 AM
I am using SW4STM32 (an Eclipse Variant) to code and debug my firmware, which is based on sample codes in package STM32Cube_FW_F4_V1.26.0.
I have observed two strange issue:
Anyone can shed some light?
2022-02-12 8:27 AM
The IDE has a different idea of the project than the compiler, although the goal is for them to be the same.
Right click project -> Index -> Rebuild.
Cleaning the project and rebuilding may also help.
2022-02-13 12:04 AM
The editor migth no longer be cpmpatible....
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.