2025-08-25 7:20 AM - last edited on 2025-08-25 7:50 AM by mƎALLEm
Split from this thread.
thanks to @Ozone @Karl Yamashita,
this afternoon I have tried to extend can2.0 to canfd with my project of stm32g474vet6. I found some strange things, I think there may be a bug of stm32g474vet6 fdcan module.
I modifed the FDCAN_TxHeader to FD_Frame and datelength to 64byte. for FDCAN_RxHeader, almost nothing to modify. then i used an app on PC to send a 64bytes CAN message, then my code received the 64bytes message and copied to rxbuffer, the rxbuffer had 64bytes data, but FDCAN_RxHeader.datalength is 15. it is not 64.
i think this is a bug of stm32g474vet6, it received 64bytes data but FDCAN_RxHeader.datalength is 15. I have no can tool now (with used by other people), when i have the can tool, i will take screenshot to show the strange thing.
hello @mƎALLEm @Saket_Om did you meet FDCAN received 64bytes but FDCAN_RxHeader.datalength is 15? is there some configuration I miss?
Thanks a lot!
Solved! Go to Solution.
2025-08-25 7:33 AM - edited 2025-08-25 7:39 AM
@dqsh06 wrote:
hello @mƎALLEm @Saket_Om did you meet FDCAN received 64bytes but FDCAN_RxHeader.datalength is 15? is there some configuration I miss?
This is not a bug and the information is provided in the reference manual RM0440 Rev 9:
DLC=15 means 64 bytes!
2025-08-25 7:33 AM - edited 2025-08-25 7:39 AM
@dqsh06 wrote:
hello @mƎALLEm @Saket_Om did you meet FDCAN received 64bytes but FDCAN_RxHeader.datalength is 15? is there some configuration I miss?
This is not a bug and the information is provided in the reference manual RM0440 Rev 9:
DLC=15 means 64 bytes!
2025-08-25 7:57 AM
When using ST's data structure for FDCAN_RxHeaderTypeDef, you should look what the reference is for DataLength, which they reference FDCAN_data_length_code
/**
* @brief FDCAN Rx header structure definition
*/
typedef struct
{
uint32_t Identifier; /*!< Specifies the identifier.
This parameter must be a number between:
- 0 and 0x7FF, if IdType is FDCAN_STANDARD_ID
- 0 and 0x1FFFFFFF, if IdType is FDCAN_EXTENDED_ID */
uint32_t IdType; /*!< Specifies the identifier type of the received message.
This parameter can be a value of @ref FDCAN_id_type */
uint32_t RxFrameType; /*!< Specifies the the received message frame type.
This parameter can be a value of @ref FDCAN_frame_type */
uint32_t DataLength; /*!< Specifies the received frame length.
This parameter can be a value of @ref FDCAN_data_length_code */
uint32_t ErrorStateIndicator; /*!< Specifies the error state indicator.
This parameter can be a value of @ref FDCAN_error_state_indicator */
uint32_t BitRateSwitch; /*!< Specifies whether the Rx frame is received with or without bit
rate switching.
This parameter can be a value of @ref FDCAN_bit_rate_switching */
uint32_t FDFormat; /*!< Specifies whether the Rx frame is received in classic or FD
format.
This parameter can be a value of @ref FDCAN_format */
uint32_t RxTimestamp; /*!< Specifies the timestamp counter value captured on start of frame
reception.
This parameter must be a number between 0 and 0xFFFF */
uint32_t FilterIndex; /*!< Specifies the index of matching Rx acceptance filter element.
This parameter must be a number between:
- 0 and (SRAMCAN_FLS_NBR-1), if IdType is FDCAN_STANDARD_ID
- 0 and (SRAMCAN_FLE_NBR-1), if IdType is FDCAN_EXTENDED_ID */
uint32_t IsFilterMatchingFrame; /*!< Specifies whether the accepted frame did not match any Rx filter.
Acceptance of non-matching frames may be enabled via
HAL_FDCAN_ConfigGlobalFilter().
This parameter can be 0 or 1 */
} FDCAN_RxHeaderTypeDef;
You can see how they defined the values
/** @defgroup FDCAN_data_length_code FDCAN Data Length Code
* @{
*/
#define FDCAN_DLC_BYTES_0 ((uint32_t)0x00000000U) /*!< 0 bytes data field */
#define FDCAN_DLC_BYTES_1 ((uint32_t)0x00010000U) /*!< 1 bytes data field */
#define FDCAN_DLC_BYTES_2 ((uint32_t)0x00020000U) /*!< 2 bytes data field */
#define FDCAN_DLC_BYTES_3 ((uint32_t)0x00030000U) /*!< 3 bytes data field */
#define FDCAN_DLC_BYTES_4 ((uint32_t)0x00040000U) /*!< 4 bytes data field */
#define FDCAN_DLC_BYTES_5 ((uint32_t)0x00050000U) /*!< 5 bytes data field */
#define FDCAN_DLC_BYTES_6 ((uint32_t)0x00060000U) /*!< 6 bytes data field */
#define FDCAN_DLC_BYTES_7 ((uint32_t)0x00070000U) /*!< 7 bytes data field */
#define FDCAN_DLC_BYTES_8 ((uint32_t)0x00080000U) /*!< 8 bytes data field */
#define FDCAN_DLC_BYTES_12 ((uint32_t)0x00090000U) /*!< 12 bytes data field */
#define FDCAN_DLC_BYTES_16 ((uint32_t)0x000A0000U) /*!< 16 bytes data field */
#define FDCAN_DLC_BYTES_20 ((uint32_t)0x000B0000U) /*!< 20 bytes data field */
#define FDCAN_DLC_BYTES_24 ((uint32_t)0x000C0000U) /*!< 24 bytes data field */
#define FDCAN_DLC_BYTES_32 ((uint32_t)0x000D0000U) /*!< 32 bytes data field */
#define FDCAN_DLC_BYTES_48 ((uint32_t)0x000E0000U) /*!< 48 bytes data field */
#define FDCAN_DLC_BYTES_64 ((uint32_t)0x000F0000U) /*!< 64 bytes data field */
2025-08-25 7:36 PM
2025-08-25 10:29 PM
CAN FD is a different standard.
It is an extension of standard CAN, but with necessary differences to differentiate between both kinds of nodes, and to facilitate higher baudrates.
You can run a CAN FD network instead, if those improvements help you.
Although I would avoid a network mixing both kinds of nodes, especially if you have no real expertise with CAN.
On a related note, I would recommend the CiA (Can in Automation) organisation and website in this regard : https://www.can-cia.org/
They have a lot of documents and expertise in this field, including CAN FD and CAN XL, although not everything for free.
2025-08-26 5:46 PM
hello @Ozone ,
Thanks for your reply!
as my project situation, this is a new project and no legacy CAN network and CAN nodes, I am the architect and I am the designer, I can choose to use CANFD or CAN2.0, what i like, what it is. so I will try to use CANFD with the benefit of 64bytes payload.
I will check https://www.can-cia.org/
thank you!
2025-08-26 10:29 PM
That is ok, if your environment and bus lengths allows for it.
As mentioned, for our application it makes no sense, we can't even reach the 1 MBit rate of standard CAN. Besides the compatibility issue.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.