STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_QSPI_AutoPolling_* delay between command and response

Hi All,I'm using a STM32H7 MCU with a ISSI IS25LP256D serial flash chip. (32MB.)I wrote a driver using a simple microcontroller and was able to read the Status Register by adding a 8uSec pause after the 0x05 command and the clock pulses to get the r...

Resolved! I've got a very strange situation on my STM32G0B0VE GPIO pin A8 gets to be the inverted signal of what PA9 is (it doesn't matter what PA9 is it can be output or Tx of Uaert1). I've checked the errata sheets. See details for more information...

I've made a software so small that it does only the following steps:1) init clock and everything to work.2) in the main program I set PIN GPIO_A_8 to input with pull up enabled, nothing is connected to that pin except for a scope probe.3) then I conf...

SCous.1 by Associate II
  • 3100 Views
  • 6 replies
  • 0 kudos

Resolved! FLASH Memory erase sector

Hello folk, i hope you fine, i am using the STM32L072, i need erase FLASH memory from 0x08008000 up to the end, i read in the datasheet that every sector has 4Kb and every page has 128 bytes, i have the following: FLASH_EraseInitTypeDef borrat;   ...

RComa.1 by Associate II
  • 3423 Views
  • 2 replies
  • 0 kudos

Resolved! __nop() taking more than one clock cycle?

I decided to run an experiment on my STM32F767ZI microcontroller. I turned on the cycle count register (DWT->CYCCNT) and decided to run the program step by step on Keil. I set the clock to the maximum amount possible with a PLL on this MCU, which is ...

IJoe.1 by Associate II
  • 6017 Views
  • 4 replies
  • 1 kudos

Resolved! STM32G484VE - GPIO status while powering on.

I have designed a target board based on STM32G484VE and I am encountering a problem with GPIO outputs while powering on.The requirement is no output should get high status while powering on or during reset. So I have configured the IOs using CUBEMX ...

BSUJA.1 by Associate
  • 1519 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.