STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Use BitBand-Adress to feed DMA ?

Hello all, basicly I want to transfer 32bit data bit-wise to a periphal address. Therefore I tried a 200 IQ move and fed the DMA with the bitband adress of the 32Bit data.But the DMA directly sets the error flag. I didn't found a hint in the data she...

0693W00000LxusuQAB.png
FKaes.1 by Associate III
  • 2317 Views
  • 3 replies
  • 0 kudos

Writing full flash page does not work

Hi !I try to write 2048 Bytes at once to flash.I do a page erase first of page 31.EraseInitStruct.TypeErase = FLASH_TYPEERASE_PAGES; EraseInitStruct.Banks = FLASH_BANK_1 ; EraseInitStruct.Page = 31; EraseInitStruct.NbPages = 1;the description o...

sde c.1 by Senior II
  • 7165 Views
  • 12 replies
  • 1 kudos

STM32G0C1CE ADC1_IN15 setup

HiTrying to configure a 48-pin STM32G0C1CE project in STMCubeIDE 1.9.0., specifically configuring pin 23/PB11 as ADC1_IN15. The embedded MX tool chip pinout view allows one to select pin 23 as ADC1_IN15, but then leaves PB11 yellowed in the overall ...

DPaul.2 by Associate II
  • 1645 Views
  • 1 replies
  • 0 kudos

Resolved! [SOLVED] SCK idling high when SPI module is stopped

 FIX: Enable pull-down resistor in SCK pinInit parameters:CPOL=0 CPHA =0, so SCK level should be idling at LOW level.Software NSSHalf-Duplex, master modeSoftware: CubeIDE 1.9, CubeMX 6.5.0Device: STM32F411CEIssue:Regardless of the clock config, SCK i...

0693W00000LxuCUQAZ.png

STm32f401 interface to mpu9250 is not working?

I am using the STm32f401 interface mpu9250 sensor with i2c communication.accelerometer and gyro values are getting, but magnetometer is not working(constant values getting),WHO AM I register getting 0x75 instead of 0x71.Regards,naren

Nredd.1 by Associate III
  • 2790 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.