STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

INVSTATE hard fault with SPI interrupt handler. STM32F405

I'm attempting to have my program run some code when a SPI transfer is complete using the RXNE flag. Setting the RXNEIE bit invokes SPI2_IRQHandler() as expected but it always results in a hard fault (CFSR register = 0x20000), without any additions t...

AWats.4 by Associate II
  • 2861 Views
  • 2 replies
  • 0 kudos

MCO capability

I'm working on a board redesign due to supply chain issue with a NXP MK70 MCU. The previous design clocked both the MK70 and a Spartan 6 FPGA with an external 50MHz crystal oscillator.The new design is using the STM32L4R9AII6 MCU -- max HSE input fre...

RussP by Associate II
  • 2854 Views
  • 4 replies
  • 0 kudos

Resolved! STM32G4 DMAMUX

Hello,Can you help me to use the DMAMUX in the STM32G474 microcontroller?How can I program the uC to make TIM2_CH1 sends a DMA request when CC. I have found this in the reference manual but I can't undesrtand which channel of the DMA is involved. Tha...

0693W00000LvzUZQAZ.png
Tommino by Senior
  • 8277 Views
  • 21 replies
  • 0 kudos

Measuring capacitance STM32L0-Disco

I'm trying to measure capacitance with my STM32L053-DiscoI'm using ADC and one output pin to charge the capacitor. I tried measuring time it takes for capacitor to charge to 62.3%.The problem that I'm facing is that the values that I'm getting from A...

0693W00000NpgdJQAR.png 0693W00000NpgdJQAR.png
JRubė.1 by Associate II
  • 6202 Views
  • 13 replies
  • 0 kudos

STM32G070 as the alternative to STM32G081

ST has confirmed that STM32G070 uses same silicon as STM32G081, thus we're considering use it as the alternative to STM32G081 due to availability problems.STM32G070 lacks BOR feature and CEC hw block acc. to datasheet but we have proven by trial that...

LPiro.1 by Associate II
  • 3035 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.