STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4P5CET ADC freezes at high noise environment

I'm using an STM32L4 for a solar inverter control project to control some H-bridges and sense some voltage and current. I run into this particular issue that when the environment is noisy (the DC input to the H-bridge is high), the ADC sometimes will...

FChen.3 by Associate
  • 2665 Views
  • 3 replies
  • 0 kudos

Wrong SVD file for STM32G491 device

TIM20 peripheral is missing in the SVD file for STM32G491 deployed in Keil PACK STM32G4xx_FDP v1.4.0Please see the attached fix with all files rebuilt (SFR and SFD)

CChiesa by Associate
  • 893 Views
  • 0 replies
  • 0 kudos

Problem with USART Communication during updates

 I am using an STM32L4 chip that sends an update to the nRF52832 on a ublox module over USART. I assume the nordic chip is in the bootloader during the update.We get a UART error: 4 and when we observe the UART lines we see that on the TX line of the...

0693W00000NpDg4QAF.png 0693W00000NpDgJQAV.png 0693W00000NpDgTQAV.png
Hueli.1 by Associate III
  • 1499 Views
  • 3 replies
  • 0 kudos

STM32H743: BDMA channel for SAI interface does not work.

I would like to use SAI interface, but the initial setup seems to be failing. ErrorHandler was called because of FIFO is Empty after calling HAL_SAI_Transmit_DMA().​The SAI is set up as follows: hsai_BlockA4.Instance = SAI4_Block_A; hsai_BlockA4.I...

Mapyam by Associate II
  • 2162 Views
  • 4 replies
  • 0 kudos

Interupt driven uart reception not working

Hi all iam working in stm32 f051c8tx microcontroller im trying to recieve a byte and if i recieve a byte in intrupt im printing "hello world " via tx of the same uart, the issue is im not able to recieve any char the below is the code any thoughts p...

NJP.1 by Associate III
  • 4630 Views
  • 10 replies
  • 0 kudos

Stm32 Header for binary files

Hello everyone,​we have to uart bootloader for stm32 mcu application. We update binary files with uart bootloader. But we need stm32 header for binary files. ​There are multiple binary files and Multiple devices that I have loaded with uart from the ...

akesk by Associate II
  • 2893 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.