2022-05-10 7:28 AM
2022-05-10 10:09 AM
Not sure which STM32 part you're using specifically.
Most support External Timer modes, using ETR or CHx as a counting clock source, similarly Encoder Modes with CH1/CH2
Most of the HAL examples have at least one using an external source, some have internal mappings to LSE/LSI
I can't say I'm familiar with external halogen timers.
This is an example using the older SPL implementation
// STM32F429I-DISCO TIM3 (CH1 PA6) External Count Demo - sourcer32@gmail.com
#include "stm32f429i_discovery.h"
//****************************************************************************
void GPIO_Configuration(void)
{
GPIO_InitTypeDef GPIO_InitStructure;
/* GPIOA clock enable */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
/* pin configuration */
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_DOWN;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource6, GPIO_AF_TIM3); // PA6 TIM3_CH1
}
//****************************************************************************
void TIM3_Configuration(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
int i;
/* Enable TIM3 Peripheral clock */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_Period = 100 - 1; // 100 (16-bit counter)
TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
TIM_TIxExternalClockConfig(TIM3, TIM_TIxExternalCLK1Source_TI1, TIM_ICPolarity_Rising, 0);
TIM_Cmd(TIM3, ENABLE);
// Likely will interrupt initially unless we clear it
for(i=0; i<3; i++)
if (TIM_GetITStatus(TIM3, TIM_IT_Update) != RESET)
TIM_ClearITPendingBit(TIM3, TIM_IT_Update);
TIM_ITConfig(TIM3, TIM_IT_Update, ENABLE);
// Could also use compare mode, set the counter maximal and advance CCRx 100 ticks at a time
}
//****************************************************************************
void TIM3_IRQHandler(void)
{
if (TIM_GetITStatus(TIM3, TIM_IT_Update) != RESET)
{
TIM_ClearITPendingBit(TIM3, TIM_IT_Update);
/* Toggle LED3 */
STM_EVAL_LEDToggle(LED3);
}
}
//****************************************************************************
void NVIC_Configuration(void)
{
NVIC_InitTypeDef NVIC_InitStructure;
/* Enable the TIM3 global Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = TIM3_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
}
//****************************************************************************
int main(void)
{
/* Initialize Leds mounted on STM32F429I-DISCO board */
STM_EVAL_LEDInit(LED3);
/* Turn on LED3 */
STM_EVAL_LEDOn(LED3);
NVIC_Configuration();
GPIO_Configuration();
TIM3_Configuration();
while(1); // Do not exit
}
//******************************************************************************
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* User can add his own implementation to report the file name and line number,
ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* Infinite loop */
while (1)
{
}
}
#endif
//******************************************************************************
2022-05-10 10:24 AM
HAL, something along the lines of
TIM_HandleTypeDef htim4;
TIM_ClockConfigTypeDef sClockSourceConfig;
TIM_MasterConfigTypeDef sMasterConfig;
htim4.Instance = TIM4;
htim4.Init.Prescaler = 0;
htim4.Init.CounterMode = TIM_COUNTERMODE_UP;
htim4.Init.Period = 65535;
htim4.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
HAL_TIM_Base_Init(&htim4);
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_ETRMODE2;
sClockSourceConfig.ClockPolarity = TIM_CLOCKPOLARITY_NONINVERTED;
sClockSourceConfig.ClockPrescaler = TIM_CLOCKPRESCALER_DIV1;
sClockSourceConfig.ClockFilter = 0;
HAL_TIM_ConfigClockSource(&htim4, &sClockSourceConfig);
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
HAL_TIMEx_MasterConfigSynchronization(&htim4, &sMasterConfig);
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.