STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Volts above VCC are dangerous for the ADC

Hi, I’m using a STM32F407G-DISC1 board which has 3V power supply.An ADC measures output of op amp. Output voltage is clamped with 3.3V Zener diode. Is the additional 0.3 volts above VCC dangerous for the ADC?

AAbd.1 by Associate
  • 1984 Views
  • 2 replies
  • 0 kudos

Reading ADC with STM32H750 Discovery Kit

i want to read out a single ADC (temperature sensor) via polling method and want to display the result on the Display. On the backside of the board are some standard arduino connectors, i used them to connect the temperature sensor (CN7 -> A0 -> PC0 ...

0693W00000QKRjXQAX.png
RHerg.1 by Associate
  • 1305 Views
  • 1 replies
  • 0 kudos

STM32 I2C, IsDeviceReady Error

Trying to communicate over I2C but keep getting error when using HAL_I2C_IsDeviceReady(). I am using a device from acconeer (XM132/XE132) which has MCU (STM32G071CBU6). Im gonna communicate the radar on the device (A111). Datasheets for the XM132 dev...

SKvan.1 by Associate
  • 916 Views
  • 0 replies
  • 0 kudos

Resolved! Regarding STM32G431MBTx board flash memory read protection.

Good Morning,I am using STM32 board with on board debugger. I can build the code as well as Flash the code in Flash memory but not able to read the code from flash memory.I want to unlock the STM32 with J-link. Please guide me.In STM32 Level 0, Level...

AWalu.3 by Associate II
  • 2460 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.