2022-07-05 10:07 PM
Good Morning,
I am using STM32 board with on board debugger. I can build the code as well as Flash the code in Flash memory but not able to read the code from flash memory.
I want to unlock the STM32 with J-link. Please guide me.
In STM32 Level 0, Level 1, Level 2 flash memory read/write protections are there.
How to check particular register value to verify level of protection.
and If it is in Level 1 how how bring back to level 0?
Please check the log messages in below attached image file(after flashing the code in flash memory).
I am not able to run the code in debug mode.
Solved! Go to Solution.
2022-07-06 4:00 PM
> I want to unlock the STM32 with J-link. Please guide me.
Apparently using the J-Link STM32 Unlock tool is hard to think of...
2022-07-06 4:00 PM
> I want to unlock the STM32 with J-link. Please guide me.
Apparently using the J-Link STM32 Unlock tool is hard to think of...
2022-07-06 9:14 PM
Thank You!
With the help of "J-Link STM32 Unlock" utility flash memory unlock issue get solved.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.