2022-07-06 11:23 PM
Trying to communicate over I2C but keep getting error when using HAL_I2C_IsDeviceReady(). I am using a device from acconeer (XM132/XE132) which has MCU (STM32G071CBU6). Im gonna communicate the radar on the device (A111). Datasheets for the XM132 device: https://developer.acconeer.com/download/xm132-module-software-user-guide-pdf/
https://developer.acconeer.com/download/xm132-datasheet-pdf/
I cant figure out why it keeps giving me error, when i have tried the possible addresses. Can anyone spot something wrong, could it be the configuration? I think the right address should be 0x51, left shifted, but have also used counter to check. Most of the code is generated from CubeMX.
int main(void)
{
/* USER CODE BEGIN 1 */
// HAL_StatusTypeDef ret;
// uint8_t buf[12];
// int16_t val;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_I2C1_Init();
MX_RTC_Init();
MX_SPI1_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
MX_DAC1_Init();
/* USER CODE BEGIN 2 */
HAL_I2C_MspInit(&hi2c1);
HAL_DAC_Start(&hdac1, DAC_CHANNEL_1);
uint16_t counter;
HAL_StatusTypeDef IDR_Result;
uint8_t I2C_Address;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
for(counter = 0 ; counter < 255; counter++){
IDR_Result = HAL_I2C_IsDeviceReady(&hi2c1, (uint16_t)(counter<<1), 3, 100);
if(IDR_Result == HAL_OK){
printf("DONE");
I2C_Address = counter;
}
}
/* USER CODE BEGIN 3 */
EnableBootLoader();
// Delay in order to handle rampup of voltage from buck converter
HAL_Delay(10);
pin_state_t id_gpio1 = GetPinState(GPIOB, GPIO_PIN_13);
printf("PB13: %s\n", id_gpio1 == PIN_STATE_LOW ? "LOW" : id_gpio1 == PIN_STATE_HIGH ? "HIGH" : "FLOAT");
//acconeer_main(0, NULL);
//while (1)
//;
}
/* USER CODE END 3 */
}
static void MX_I2C1_Init(void)
{
/* USER CODE BEGIN I2C1_Init 0 */
/* USER CODE END I2C1_Init 0 */
/* USER CODE BEGIN I2C1_Init 1 */
/* USER CODE END I2C1_Init 1 */
hi2c1.Instance = I2C1;
hi2c1.Init.Timing = 0x10707DBC;
hi2c1.Init.OwnAddress1 = 164;
hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
hi2c1.Init.OwnAddress2 = 0;
hi2c1.Init.OwnAddress2Masks = I2C_OA2_NOMASK;
hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
if (HAL_I2C_Init(&hi2c1) != HAL_OK)
{
Error_Handler();
}
/** Configure Analogue filter
*/
if (HAL_I2CEx_ConfigAnalogFilter(&hi2c1, I2C_ANALOGFILTER_ENABLE) != HAL_OK)
{
Error_Handler();
}
/** Configure Digital filter
*/
if (HAL_I2CEx_ConfigDigitalFilter(&hi2c1, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN I2C1_Init 2 */
/* USER CODE END I2C1_Init 2 */
}
void HAL_I2C_MspInit(I2C_HandleTypeDef* hi2c)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
if(hi2c->Instance==I2C1)
{
/* USER CODE BEGIN I2C1_MspInit 0 */
/* USER CODE END I2C1_MspInit 0 */
__HAL_RCC_GPIOB_CLK_ENABLE();
/**I2C1 GPIO Configuration
PB6 ------> I2C1_SCL
PB7 ------> I2C1_SDA
*/
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
GPIO_InitStruct.Pull = GPIO_PULLUP;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; //GPIO_SPEED_FREQ_LOW;
GPIO_InitStruct.Alternate = GPIO_AF6_I2C1;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
/* Peripheral clock enable */
__HAL_RCC_I2C1_CLK_ENABLE();
/* I2C1 DMA Init */
/* I2C1_RX Init */
hdma_i2c1_rx.Instance = DMA1_Channel5;
hdma_i2c1_rx.Init.Request = DMA_REQUEST_I2C1_RX;
hdma_i2c1_rx.Init.Direction = DMA_PERIPH_TO_MEMORY;
hdma_i2c1_rx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_i2c1_rx.Init.MemInc = DMA_MINC_ENABLE;
hdma_i2c1_rx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_i2c1_rx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_i2c1_rx.Init.Mode = DMA_NORMAL;
hdma_i2c1_rx.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_i2c1_rx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hi2c,hdmarx,hdma_i2c1_rx);
/* I2C1_TX Init */
hdma_i2c1_tx.Instance = DMA1_Channel6;
hdma_i2c1_tx.Init.Request = DMA_REQUEST_I2C1_TX;
hdma_i2c1_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
hdma_i2c1_tx.Init.PeriphInc = DMA_PINC_DISABLE;
hdma_i2c1_tx.Init.MemInc = DMA_MINC_ENABLE;
hdma_i2c1_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_BYTE;
hdma_i2c1_tx.Init.MemDataAlignment = DMA_MDATAALIGN_BYTE;
hdma_i2c1_tx.Init.Mode = DMA_NORMAL;
hdma_i2c1_tx.Init.Priority = DMA_PRIORITY_LOW;
if (HAL_DMA_Init(&hdma_i2c1_tx) != HAL_OK)
{
Error_Handler();
}
__HAL_LINKDMA(hi2c,hdmatx,hdma_i2c1_tx);
/* I2C1 interrupt Init */
HAL_NVIC_SetPriority(I2C1_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(I2C1_IRQn);
/* USER CODE BEGIN I2C1_MspInit 1 */
/* USER CODE END I2C1_MspInit 1 */
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.