STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GPIO state Of STM32L071

Hi,I am using STM32L071CBT6 with VDD,VDDA,VDDIO2 supply Voltage of 1.8V , Please refer above image, i am using PB6 as GPIO ,initially it is configured as push-pull output , we are getting 0 to 2V output swing, when we changed GPIO to Open Drain with ...

0693W00000QKT9pQAH.png
SJ.8 by Associate
  • 1497 Views
  • 1 replies
  • 0 kudos

STM32F7 supply issues

Hi, We currently have a project where we use STM32F767NIH6, customer is concerned that the part is not available with long lead times. When do you see the supply issue returning to normality? There has been no news or statements made by ST on the iss...

markH by Associate III
  • 1481 Views
  • 1 replies
  • 0 kudos

Issue with nucleo L476RG and ADC and DMA with a 500KHz signal

Hello, I try to use a nucleo to acquire a signal at 500KHz but I can't.I already use this code to acquire a 30KHz signal with DMA a 1MHz sampling and it's OK.now I try to with a wampling at 1MHZ, 10MHz, the acquire signal isn't the good one. Value fl...

Seth1er by Associate II
  • 1562 Views
  • 1 replies
  • 0 kudos

Resolved! FDCAN1 and FDCAN2 in STM32G0B1RCI6N

Hi, I configured FDCAN1 in classic format and was able to send CAN messages to a recipient. However, if I want to try the same with FDCAN2 it does not work and the TX FIFO gets full and goes to the error handler. However, If I change FDCAN_Config to ...

STM32H7 Segger J-Link Debugging Issue

Hello,When trying to do a debug session onto these different STM32H7 devices:STM32H743IIT6 / STM32H753IIT6STM32H7A3IGT6we are receiving the errorwith the following console statements:SEGGER J-Link GDB Server V7.62a Command Line Version   JLinkARM.dll...

0693W00000QKUdHQAX.png 0693W00000QKUdqQAH.png
MPete.3 by Associate II
  • 5084 Views
  • 6 replies
  • 0 kudos

Possible error in Cortex-M0 programming manual.

Cortex-M0 programming manual have several instructions like this:You can use the LSR ...When the instruction is LSRS, the carry flag is updated ...But I believe that on Cortex-M0, there is no optional 'S' appended to instructions to update flags. Ins...

AA1 by Senior III
  • 3406 Views
  • 5 replies
  • 0 kudos

Resolved! STM32G0 ADC 16-bit oversampling example

Hi,I'm not able to find any example on STM32CubeIDE about ADC 16-bit oversampling. Could someone from ST provide this for the STM32G0 MCUs?thanks in advance,gaston

Gaston by Senior
  • 3209 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.