STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PWM capture with TIMER (with DMA)

I have configured TIMER2 to capture PWM input (Basically PWM inputmode). Both CCR1 and CCR2 captures period and ontime of the PWM signal respectively. I configured DMA to captures these two registers CCR1 and CCR2 by configuring array of two 32bit bu...

Shakthi by Associate II
  • 3135 Views
  • 4 replies
  • 0 kudos

RTC Initialization have a problem.

HiI created my new project follow SubGHz Phy Ping Pong example project. This is my MX_RTC_Init() function:void MX_RTC_Init(void) {   /* USER CODE BEGIN RTC_Init 0 */   /* USER CODE END RTC_Init 0 */   RTC_TimeTypeDef sTime = {0}; RTC_DateType...

[STM32H745xI/G] what means the "VOS0 and VOS1 are not available for industrial temperature range", STM32H745xxx3 sales types

quote "For STM32H745xxx3 sales types (industrial temperature range) the voltage regulator output can be set only to VOS2 or VOS3 in Run mode (VOS0 and VOS1 are not available for industrial temperature range)." from st.com/resource/en/datasheet/stm32h...

SLiu.61 by Associate II
  • 4300 Views
  • 5 replies
  • 1 kudos

Setting timer 1 channel 4 high on startup

I am using Timer 1 DMA to generate a waveform. The generation part works fine, but the waveform is inverted, so I need to set channel 4 (output of CC4) signal high during initialization. I have tried a bunch of thing, my latest attempt is below. W...

JMala.3 by Associate III
  • 4226 Views
  • 8 replies
  • 0 kudos

Hello, I have three STM32F469I-DISCO boards that I need to be fully synchronized. As I searched, the best way to do this is by making them all operate with the same clock. How can I do this? Please help.

I read that this is possible by using an external clock or making two of them connected to the third board's clock. However, I do not know how to implement this. Please assist.

RAlna.1 by Associate
  • 2539 Views
  • 6 replies
  • 0 kudos

STM32F207 Timer counter fails to increment

I am developing an application on STM32F207ZC MCU with the internal oscillator as the clock source. I am trying to use two hardware timers(Timer 4 and Timer 9) to generate PWM signals in GPIO pins. I am able to produce the PWM signals with both timer...

AJose.2 by Associate II
  • 3296 Views
  • 5 replies
  • 0 kudos

How to enable interrupt with registers

Hi,I have seen that to enable the interrupt for a given peripheral we must enable the correct bit in the peripheral registers (e.g in the DIER register for a timer) and then call the following functions (e.g for peripheral timer3)  NVIC_EnableIRQ(TIM...

Tommino by Senior
  • 3773 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.