2022-07-20 4:19 AM
I have configured TIMER2 to capture PWM input (Basically PWM inputmode). Both CCR1 and CCR2 captures
period and ontime of the PWM signal respectively.
I configured DMA to captures these two registers CCR1 and CCR2 by configuring array of two 32bit buffer in DMA_SM0AR.
The register DMA_SPAR is configured with CCR1 address. The number of transacctions configured in DMA_SNDTR is two.
MCU: STM32F207IEH6
The configs are as below,
// Module number DMA1
// Stream. - 6
// Channel - 3
// Memory data size - 32 bit
// Peripheral data size - 32 bit
// direction - Peripheral to memory
// FIFO mode Direct
// FIFO threshold not used
// Double buffer mode - off
// Circular mode - on
// PINC - on
// MINC - on
I understand that whenever there is an event for raising edge/falling edge the counter values captured in CCR1 or CCR2 copied to the address in DMA_SM0AR.
ie, transfer 1. CCR1 - transfer from Peripheral (TIMER2) to Memory
transfer 2. CCR2 - transfer from Peripheral (TIMER2) to Memory
My query is, the flags HTIFx , TCIFx (in register DMA_HISR) will be set for each of the transfers (1 and 2)? or
as a whole, when transfer 1 is done the HTIFx will be set and when transfer 2 is done the TCIFx is set (because the DMA_SNDTR goes to zero when two requests are served).
Please help me understanding this.
2022-07-20 4:47 AM
DMA1 Stream6 Ch3 is triggered by TIM2_CH2, so it depends on how exactly is set TIM2_CH2 - if it's set to capture on both edges, then there will be a transfer upon each edge, but I doubt you've set it so.
I personally would set up two DMAs, one triggered by CH1 and other by CH2, both storing data to a different array.
JW
2022-07-20 5:15 AM
The capture done on both raising (Captures CCR1 and clears the counter) and falling edge ( captures CCR2).
So the flags HTIFx , TCIFx are set for each request?
The number of data transfer doesn't play role on setting this TCIFx flag.
2022-07-20 6:57 AM
@Community member The HTIFx flag will be set when DMA_SNDTR decremented to 1 and TCIFx flag set when DMA_SNDTR becomes zero.
2022-07-20 9:29 AM
> The capture done on both raising (Captures CCR1 and clears the counter) and falling edge ( captures CCR2).
Yes, but the DMA trigger comes only from CH2.
> The HTIFx flag will be set when DMA_SNDTR decremented to 1 and TCIFx flag set when DMA_SNDTR becomes zero.
Yes.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.