2022-07-19 8:25 PM
Hello! I'm uploading a code to a custom board and got the following error:
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a16184.srec
File : ST-LINK_GDB_server_a16184.srec
Size : 45.39 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 2]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.248
Verifying ...
Error: Data mismatch found at address 0x08000CB4 (byte = 0x64 instead of 0x7B)
Error: Download verification failed
Shutting down...
Exit.
Is the code uploading incorrectly? How can I fix this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.