2022-07-20 7:52 AM
Hi
I created my new project follow SubGHz Phy Ping Pong example project. This is my MX_RTC_Init() function:
void MX_RTC_Init(void)
{
/* USER CODE BEGIN RTC_Init 0 */
/* USER CODE END RTC_Init 0 */
RTC_TimeTypeDef sTime = {0};
RTC_DateTypeDef sDate = {0};
RTC_AlarmTypeDef sAlarm = {0};
/* USER CODE BEGIN RTC_Init 1 */
/* USER CODE END RTC_Init 1 */
/** Initialize RTC Only
*/
hrtc.Instance = RTC;
hrtc.Init.HourFormat = RTC_HOURFORMAT_24;
hrtc.Init.AsynchPrediv = RTC_PREDIV_A;
hrtc.Init.SynchPrediv = RTC_PREDIV_S;
hrtc.Init.OutPut = RTC_OUTPUT_DISABLE;
hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE;
hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH;
hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN;
hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE;
hrtc.Init.BinMode = RTC_BINARY_NONE;
if (HAL_RTC_Init(&hrtc) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN Check_RTC_BKUP */
if(HAL_RTCEx_BKUPRead(&hrtc, RTC_BKP_DR10) != 0x32F2)
{
/* USER CODE END Check_RTC_BKUP */
/** Initialize RTC and set the Time and Date
*/
sTime.Hours = 0x0;
sTime.Minutes = 0x0;
sTime.Seconds = 0x0;
sTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &sTime, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
sDate.WeekDay = RTC_WEEKDAY_MONDAY;
sDate.Month = RTC_MONTH_JANUARY;
sDate.Date = 0x1;
sDate.Year = 0x0;
if (HAL_RTC_SetDate(&hrtc, &sDate, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
/** Enable the Alarm A
*/
sAlarm.AlarmTime.Hours = 0x0;
sAlarm.AlarmTime.Minutes = 0x0;
sAlarm.AlarmTime.Seconds = 0x0;
sAlarm.AlarmTime.SubSeconds = 0x0;
sAlarm.AlarmTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
sAlarm.AlarmTime.StoreOperation = RTC_STOREOPERATION_RESET;
sAlarm.AlarmMask = RTC_ALARMMASK_NONE;
sAlarm.AlarmSubSecondMask = RTC_ALARMSUBSECONDMASK_NONE;
sAlarm.AlarmDateWeekDaySel = RTC_ALARMDATEWEEKDAYSEL_DATE;
sAlarm.AlarmDateWeekDay = 0x1;
sAlarm.Alarm = RTC_ALARM_A;
if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
/** Enable the Alarm B
*/
sAlarm.AlarmTime.Seconds = 0x10;
sAlarm.AlarmMask = RTC_ALARMMASK_DATEWEEKDAY|RTC_ALARMMASK_HOURS
|RTC_ALARMMASK_MINUTES;
sAlarm.Alarm = RTC_ALARM_B;
if (HAL_RTC_SetAlarm_IT(&hrtc, &sAlarm, RTC_FORMAT_BCD) != HAL_OK)
{
Error_Handler();
}
/** Enable the WakeUp
*/
if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 0, RTC_WAKEUPCLOCK_CK_SPRE_16BITS, 0) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN RTC_Init 2 */
HAL_RTCEx_BKUPWrite(&hrtc, RTC_BKP_DR10, 0x32F2);
}
/* USER CODE END RTC_Init 2 */
}First time, I write 0x32F2 to BackUp register 10. The TIMER_IF_Init() function below,
UTIL_TIMER_Status_t TIMER_IF_Init(void)
{
UTIL_TIMER_Status_t ret = UTIL_TIMER_OK;
/* USER CODE BEGIN TIMER_IF_Init */
/* USER CODE END TIMER_IF_Init */
if (RTC_Initialized == false)
{
hrtc.IsEnabled.RtcFeatures = UINT32_MAX;
/*Init RTC*/
MX_RTC_Init();
/*Stop Timer */
TIMER_IF_StopTimer();
/** DeActivate the Alarm A enabled by STM32CubeMX during MX_RTC_Init() */
HAL_RTC_DeactivateAlarm(&hrtc, RTC_ALARM_A);
/*overload RTC feature enable*/
hrtc.IsEnabled.RtcFeatures = UINT32_MAX;
/*Enable Direct Read of the calendar registers (not through Shadow) */
HAL_RTCEx_EnableBypassShadow(&hrtc);
/*Initialize MSB ticks*/
TIMER_IF_BkUp_Write_MSBticks(0);
TIMER_IF_SetTimerContext();
/* Register a task to associate to UTIL_TIMER_Irq() interrupt */
UTIL_TIMER_IRQ_MAP_INIT();
RTC_Initialized = true;
}
/* USER CODE BEGIN TIMER_IF_Init_Last */
/* USER CODE END TIMER_IF_Init_Last */
return ret;
}My project run without no stuck in first time. When I reset MCU, my project stuck when called PWR_ExitStopMode().
What wrong in my code.
Anyone know how to fix this problem? Please support me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.