STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L462 configured to wake up from stop mode 2, using RXNE interrupt, not able to receive asynchronous responses sent from the modem.

STM32L462 is configured to wake up from stop 2 mode on RXNE interrupt. Since the response length is unknown and dynamic, have configured interrupt on every character till the end of character is received. MCU is successfully waking up on UART recepti...

KK.4 by Associate II
  • 1115 Views
  • 1 replies
  • 0 kudos

Resolved! How to init SPI properly

Hi,I am trying to init SPI1 (to just receive data qwith MISO) on nucleo G474RE without using HAL libraries.Can you help me to assess why my code does not work ? I can't see the clock eventhough SPI1 is enabled void SPI1_init(){ RCC-> APB2ENR|=(1 AHB...

_legacyfs_online_stmicro_images_0693W00000QLmdH.png _legacyfs_online_stmicro_images_0693W00000QLmdR.png
Tommino by Senior
  • 8913 Views
  • 20 replies
  • 0 kudos
rwils.1 by Associate III
  • 2823 Views
  • 6 replies
  • 0 kudos

Resolved! How to connect STM32F407G-DISC1 by SWD to JTrace Pro / JLink

Hello,I have an STM32F407G-DISC1 evaluation board which I have been trying to connect to through SWD with a Segger JTrace Pro, but I haven't been able to connect to the board for some reason. I have been following a Segger provided document for the c...

DLlan.1 by Associate II
  • 3888 Views
  • 6 replies
  • 0 kudos

STLINK_V3 SET how to use for Custome board?

Hello, I am working on STM32H7 . I have custome board , I have to use the STLINK_V3 SET, which things that I need to consider for the programming through STLINK. How much vtg I have to set 3V/5V , In stm32Cube ide which setting I have to make. Can u ...

MDeva.1 by Associate II
  • 862 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.