2022-07-23 10:51 AM
Hello,
I am working on STM32H7 . I have custome board , I have to use the STLINK_V3 SET, which things that I need to consider for the programming through STLINK. How much vtg I have to set 3V/5V , In stm32Cube ide which setting I have to make. Can u please help me
2022-07-23 3:07 PM
The H7 is running at 3V or 3.3V
SWD connection, you want SWDIO, SWCLK, NRST and GND.
Should be able to check connectivity using STM32 Cube Programmer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.