STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CPU halted during flash erase opertaion

I am facing CPU halt during flash erase opertaion, so i chosen RAM linker script "STM32F769NIHX_RAM.ld" to enable code execute from RAM. Now the code and data section of my software is purely working from RAM (no fash access required) but CPU is halt...

sm.4 by Associate
  • 2135 Views
  • 3 replies
  • 0 kudos

Resolved! Which model in an ibis model file should I use?

Currently I am trying to use ibis model for simulation. I found ibis model file provided by STMicro and try to use them. But I could not figure out which model pointed by model selector I should use. For example, there are 24 candidates of the model ...

SShir.2 by Associate II
  • 1809 Views
  • 2 replies
  • 0 kudos

Cmake issue: Too many levels of symbolic links

Hi all!Currently, I create one project STM32F103 MCU with RTOS by Cmake and I got the issue when I compile the project. That is "Too many levels of symbolic links".My cmake version is 3.22.1.I would like to send you my CMakelists.txt file. Please che...

PTuan.1 by Associate
  • 1332 Views
  • 0 replies
  • 0 kudos

Resolved! About Pin function

I would like to do UART communication using nucleo l4r5zi.I would like to do the pin setting, but I do not know how to do that.​Please let me ask the following two questions here.1.Is my understanding correct that the pin settings for CN7, CN8, CN9 a...

Myasu.1 by Senior
  • 5105 Views
  • 2 replies
  • 0 kudos

DfuSe Demo v3.0.6 doesn't flash stm32f722ret6

I was trying to flash stm32f722ret6 via DFU mode. DfuSe Demo typing successful status but firmware doesn't update.But when I download .hex file via ST-LINK a firmware works. What could be the problem?

0693W00000QNm4kQAD.jpg 0693W00000QNm59QAD.jpg
ab.2 by Associate II
  • 5064 Views
  • 11 replies
  • 0 kudos

Error in writing RTC time & date into internal flash

Hello,I am working on a project in which i have to save my sensor readings in STM32G030F6's internal flash memory with time stamps. For that i am using STM's internal RTC to get the time and date. But problem is that i can't write data into flash if ...

Resolved! Is it possible on STM32H730 (or any) to switch between classical CAN and CANFD configurations during runtime?

I've been working on the STM32H730 processor and have been struggling to get the FDCAN peripherals to switch between classical CAN and CAN FD for transmissions. It seems that when I'm transmitting as classical CAN everything works fine. Then when I s...

0693W00000QNV0bQAH.png
snurb by Associate II
  • 2433 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.