2022-08-21 3:12 AM
Hi all!
Currently, I create one project STM32F103 MCU with RTOS by Cmake and I got the issue when I compile the project. That is "Too many levels of symbolic links".
My cmake version is 3.22.1.
I would like to send you my CMakelists.txt file. Please check the attachment and help me figure the issue out.
Thanks and regards
# Template CMakeLists.txt configuration for STM32 MCUS
cmake_minimum_required(VERSION 3.12)
# ##############################################################################
# Edit your MCU information up to the next border
project(nrf24l01)
set(PROJECT_DIR output)
include(${CMAKE_CURRENT_SOURCE_DIR}/gcc-arm-none-eabi.cmake)
include(${CMAKE_CURRENT_SOURCE_DIR}/source.cmake)
set(PROJECT_OUTPUT_PATH /build_outputs)
if(DEFINED PROJECT_OUTPUT_PATH)
set(BUILD_OUTPUT_DIR ${PROJECT_OUTPUT_PATH})
else()
set(BUILD_OUTPUT_DIR ${CMAKE_CURRENT_SOURCE_DIR}/../${PROJECT_TYPE}/build_outputs)
endif()
set(MCU_FAMILY STM32F1xx)
set(MCU_MODEL STM32F103x6)
set(CPU_PARAMETERS
-mcpu=cortex-m3
)
# Some default GCC settings
set(FLAGS
"-fdata-sections -ffunction-sections \
--specs=nano.specs -Wl,--gc-sections")
set(CPP_FLAGS
"-fno-rtti -fno-exceptions \
-fno-threadsafe-statics")
set(CMAKE_TRY_COMPILE_TARGET_TYPE STATIC_LIBRARY)
set(STARTUP_SCRIPT ${CMAKE_CURRENT_SOURCE_DIR}/startup_stm32f103x6.s)
set(MCU_LINKER_SCRIPT ${CMAKE_CURRENT_SOURCE_DIR}/STM32F103R6Hx_FLASH.ld)
# ##############################################################################
set(EXECUTABLE ${CMAKE_PROJECT_NAME})
# enable_language(C CXX ASM)
set(CMAKE_C_STANDARD 11)
set(CMAKE_C_STANDARD_REQUIRED ON)
set(CMAKE_C_EXTENSIONS ON)
set(CMAKE_CXX_STANDARD 20)
set(CMAKE_CXX_STANDARD_REQUIRED ON)
set(CMAKE_CXX_EXTENSIONS ON)
# Executable files
add_executable(${EXECUTABLE}
${STM32CUBEMX_SOURCES}
${PROJECT_SOURCES}
${STARTUP_SCRIPT})
# Embedded macros(defines)
target_compile_definitions(${EXECUTABLE} PRIVATE
${MCU_MODEL}
USE_HAL_DRIVER)
# Add header directories (AFTER add_executable !!)
target_include_directories(${EXECUTABLE} PRIVATE
${CUBEMX_INCLUDE_DIRECTORIES}
${PROJECT_INCLUDE_DIRECTORIES})
# Compiler and linker options
target_compile_options(${EXECUTABLE} PRIVATE
${CPU_PARAMETERS}
-Wall
-Wextra
-Wpedantic
-Wno-unused-parameter
$<$<COMPILE_LANGUAGE:CXX>:
-Wno-volatile
-Wold-style-cast
-Wuseless-cast
-Wsuggest-override>
$<$<CONFIG:Debug>:-Og -g3 -ggdb>
$<$<CONFIG:Release>:-Og -g0>)
target_link_options(${EXECUTABLE} PRIVATE
-T${MCU_LINKER_SCRIPT}
${CPU_PARAMETERS}
-Wl,-Map=${CMAKE_PROJECT_NAME}.map
--specs=nosys.specs
-Wl,--start-group
-lc
-lm
-lstdc++
-Wl,--end-group
-Wl,--print-memory-usage)
add_custom_command(TARGET ${EXECUTABLE} POST_BUILD
COMMAND ${CMAKE_SIZE} $<TARGET_FILE:${EXECUTABLE}>)
add_custom_command(TARGET ${EXECUTABLE} POST_BUILD
COMMAND ${CMAKE_OBJCOPY} -O ihex $<TARGET_FILE:${EXECUTABLE}>
${EXECUTABLE}.hex
COMMAND ${CMAKE_OBJCOPY} -O binary $<TARGET_FILE:${EXECUTABLE}>
${EXECUTABLE}.bin)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.