STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

copying a dual-core project

I have problem with duplicating an existing dual-core project in STM32CubeIDE. in single core project it was just sufficient to copy and paste a project to save it with another name. but for dual core project this doesnot work. hoe can we duplicate a...

YAtta.1 by Associate
  • 1078 Views
  • 1 replies
  • 0 kudos

CAN RX interrupt not working on STM32F303

Good day everybody, I can't get this simple CAN reception with interrupt to work on my STM32F303VC microcontroller. I have probed the TX and RX lines of the receiving side with a logic analyzer and I saw no problem, however I don't get any interrupts...

IJoe.1 by Associate II
  • 1622 Views
  • 1 replies
  • 0 kudos

Resolved! About OCTSPI

I would like to communicate with FLASH using OCTSPI on nucleo l4r5zi.   I am creating a driver for OCTSPI for communication, but I have a question.I plan to use the regular command mode, INDIRECT_READ and INDIRECT_WRITE.The driver is designed to stor...

Myasu.1 by Senior
  • 5129 Views
  • 7 replies
  • 0 kudos

Repetition of arbitrary waveform through DMA (Problem)

Hi, I created a program that should create repetition on an arbitrary waveform through DMA burst feature. I use circular mode and I decide to stop it when the repetition are done. I use the transfer complet interrupt to increment a variable to have t...

0693W00000QOBtTQAX.jpg 0693W00000QOBuMQAX.png
YSall.1 by Senior
  • 2357 Views
  • 4 replies
  • 0 kudos

STM32L4R9 OSPI auto polling won't stop

I'm using a STM32L4R9 with a W25G128, using non HAL code. The problem I'm seeing is that auto polling isn't stopped on match per logic analyzer. I have this set up to auto poll for write complete, register 0x05 busy bit 1. The match happens, I clear ...

_EFrie by Senior
  • 3975 Views
  • 10 replies
  • 0 kudos

Resolved! STM32H745 hw registers access synchronisation between cores

There is gpio interrupts enabled on both cores, but for different pins.Both cores run mbed os 6.15Programs on th both cores are almost the same:void gpioInterruptHandler () { gpio_irq_disable (); someFlag = true; disableCounter++; }   voi...

AP by Associate
  • 1141 Views
  • 2 replies
  • 1 kudos

Ground problem while reading ADC in STM32f030f4p6 module

I want to take a voltage reading over the voltage divider circuit I prepared with the STM32f030f4p6 module. I divided the voltage as 1 by 13. When I run the code in debug mode, for example, if I give 14V, I need to read 1V, but the value I see in the...

MYara.2 by Associate
  • 1314 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.