STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NUCLEO L496ZG SWO not able to make it work

HiI am trying to enable the SWO to debug with printf. I have a NUCLEO L496ZG board. The ITM_SendChar function seems to get called but no data on the ITM console. What am I doing wrong?This is the main.c code:/** *************************************...

0693W00000QO4yRQAT.png 0693W00000QO4ybQAD.png 0693W00000QO4zFQAT.png 0693W00000QO53CQAT.jpg
RPG by Senior
  • 1865 Views
  • 3 replies
  • 0 kudos

STM32L082 - Dual NVM banks (how to boot from bank2)

Dear ST experts,I am using the STM32L082 and looking to utilize the Dual Banks to be able to upgrade the firmware (swap between bank1 and bank2 and visa versa). Have compiled code for BANK1 and compiled for BANK2. Code flashed to BANK1 (0x0800 0000) ...

My STM32F105RB stop running

I uses STM32F105RB for my project. I use USART1, USART2, USART3 and UART4 to receive data from sensor. everything works normal. But after 2-3hours it stop running. I check Fault Reports it shows Memory Manage Faults and Bus Faults at some address and...

0693W00000QO2VSQA1.png 0693W00000QO2YIQA1.png
WPong.1 by Associate III
  • 1077 Views
  • 1 replies
  • 0 kudos

Resolved! Issue With dual Core Project for STM32H757 Evaluation board

Hi,I am using STM32H757 Evaluation board . I created dual core project using by referring the below linkhttps://www.youtube.com/watch?v=jI1k6p-fduEI was able to create the project and compile the same as per the instruction mentioned in the above lin...

0693W00000QNy93QAD.png

I2C does not work with SPI Slave mode on STM32L011

I want to use I2C at master mode, and SPI at slave mode.After HAL_SPI_TransmitReceive_IT api is called, HAL_I2C_Master_Transmit api does not work on STM32L011K4T6.Before HAL_SPI_TransmitReceive_IT api is called, HAL_I2C_Master_Transmit api does work ...

SUchi.4 by Associate II
  • 2721 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F105RBT6, PB3 not working as GPIO push-pull output with application using firmware package 1.8.x but works fine with similar app using firmware package 1.7.0

HiI have an application that uses an STM32F105RBT6 ant its USB peripheral as host mode connected to a HID controller, and driving a few GPIOs connected to 74HC04 inputs.The application was created using firmware package 1.7.0 and STM32CubeMx with a M...

FLACO.1 by Associate II
  • 3337 Views
  • 3 replies
  • 0 kudos

STM32G030F6 USART1 received interrupt not working

Hi I am using ​STM32G030F6 I am try to programing UART 1&2. UART2 is working fine with transmit & receive data. But UART1 only able to transmit data not able received.​Please let me is there any settings is required.​

dsapk.1 by Associate
  • 1018 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.