STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Use CAN in STM32F042F4: Can not config in CubeMX

I want to use CAN Bus in STM32F042F4 (TSSOP20). In the data sheet it says, CAN_RX on PA11 Pin 17, CAN_TX on PA12 Pin 18.When trying to configure in CubeMX, CAN function is greyed out and the pinout has not PA11 and PA12. Isn't it possible to use CAN ...

0690X000006CGhpQAG.png 0690X000006CGhuQAG.png
harald by Associate III
  • 4612 Views
  • 4 replies
  • 0 kudos

Resolved! Configurate uart without using stmcubeMx

I am currently working on a project to program a PLC. This one already has a program to control its operation. We are using the Nucleo board STM32F302RBT6. The goal is to extend the program to be able to integrate the uart communication. Unfortunatel...

TGill.4 by Associate II
  • 1825 Views
  • 3 replies
  • 0 kudos

Stm32 H7 ADC Conversion time ?

Hello I m trying measure adc conversion time , I look datasheet , f_adc=37 Mhz(for fast channel) with 12 bit resulation, 4.10 MSps , so ı use f_adc=32 Mhz(for fast channel) with 12 bit resulation, 3.54 MSps should be, but I m not measure 3.54 MSps,I ...

0693W00000GZb31QAD.jpg 0693W00000GZb2wQAD.png 0693W00000GZb2rQAD.png

Resolved! Peripheral to Mem BDMA on H750

Hi, I am looking to read 16bits which are split between port A and B on an interrupt hooked up to exti0. I *seem* to have the dma working and see the expected data at DMA completion (interrupt). However the DMA controller does not react to the interr...

VN.2 by Associate III
  • 2053 Views
  • 5 replies
  • 0 kudos

Resolved! What is Address offset?

Hello, I have a Nucleo L476RG which I'm using for different projects, and I never gave an importance to the offset addresses that are written before every register in the reference manual.Can anyone explain to me what are theses offsets.

Vertinhol by Associate III
  • 14297 Views
  • 7 replies
  • 1 kudos

STM32L562 MEM2MEM DMA complete interrupt delayed

Hello. I'm struggling with DMA on that specific MCU. I'm using MEM2MEM to transfer data from RAM to GPIOD, triggered by TIM3 interrupt. Here's my init code:void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMAMUX1_CLK_ENABLE();...

0693W00000SuHfKQAV.png
gumyns by Associate
  • 1302 Views
  • 1 replies
  • 0 kudos

STM32L4 how to get LSE clock connected with an output pin?

The output pin in question can be configured as LPTIM1_OUT and I know how to configure the LPTIM1 but I'm afraid I'll endup with LSE/2 as a clock. I need the LSE clock source to be connected to that output pin 1:1.Besides using the LPTIM1 isn't there...

RZ by Associate II
  • 2531 Views
  • 3 replies
  • 0 kudos

PWM Between 2 stm32

Hi guys,I need a help..and sorry my bad English.I would like to know how i can generate a pwm from one stm nucleo H7A3ZI-Q and read the duty cycle (generated from the first STM32) from another stm, implementing everything via simulink if possiblethan...

GCocc.1 by Associate II
  • 1624 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.