STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F303RET6 Timer PWM Output Not working as expecte

I am trying to configure a PWM output pin. Ive managed to get it working, however the results are not as expected, and i cannot understand whats happening.Currently my timer clocks are running at 64MHz.I've setup a timer with the follow values, and i...

Check free memory (STM32L0)

Hello,During code execution I would like to monitor the available memory. Is there a default function available to check the available RAM memory? Thanks

STM32-L452RE comparator triggering in both edges

Hey!I have been with a problem with the stm32l452 comparator for a few days now and I can't figure it out. The interrupt of COMP1 triggers on both edges rather than rising edge.I tried differents configurations but main is the following:hcomp1.Init.I...

PParo.2 by Associate II
  • 3661 Views
  • 1 replies
  • 0 kudos

I2C with 5 MHz - possible?

If I understand STM32H7xx datasheet, I2C peripherals support up to 1 MHz (FM, FM+), 'officially'.I would need an I2C with 5 MHz SCL clock.I tried and have 'overclocked' I2C with 2 MHz which works fine.Based on the clock configuration (e.g. a 50 MHz P...

STM32H743 interfacing with STUSB1602

HelloI need to interface a STM32H743 with a STUSB1602. I want to port STM32F072_MB1303_DRP_SRCING_DEVICE example to my STM32H743 and use it to control 5x STUSB1602. It seem like this example uses RTOS- Has anyone successful done this or can they reco...

MMevo.1 by Associate II
  • 834 Views
  • 0 replies
  • 0 kudos

Resolved! DMA not working on STM32F303RET6

I'm struggling to get DMA working on a PWM Timer. I've read just about everything i can, but not having any luck get it working.Running this code.. produces a PWM signal as expected on the output.TIM1->CCR1 = 50; HAL_TIM_PWM_Start(&htim1, TIM_CHANN...

0693W00000Su6y6QAB.png

STM32G0 - internal flash read operation returns always 0

HelloI have a const variable located in the internal flash memory. When I directly access this variable in flash, the read operation returns always 0 (even when the content of that location in flash is not 0). When I change the code to first copy the...

ADel .3 by Associate
  • 1501 Views
  • 3 replies
  • 0 kudos

Using Nucleo 429ZI and implanting a simple SPI code , There are no signals on the SCK Mosi pins when sending data on SPI1

I am using SPI1 as a Master full duplex , and checking in the Nucleo 429 zi   PA5   ------> SPI1_SCKThere is no clock , I using a scope and testing PA5 pin on the Nucleo 429 zi I attach the code , its very short code Here is the link to the pin descr...

RKore.1 by Associate II
  • 4536 Views
  • 8 replies
  • 0 kudos

STM32H7 Eval board ADC accuracy

Hello everyone,I am currently trying to get the ADC on the STM32H745ZIQ to work like it should according to the AN *Getting started with the STM32H7 Series MCU 16-bit ADC - Application note.On page 3 the spectrum is shown along with the measurement s...

0693W00000StyXvQAJ.png
krausiul by Associate
  • 3507 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.