STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32g0b1cetx flash erase example code is not working

Hello everyone I try erase and write the flash of stm32g0b1cetx series. every time I try I got this error code from flash " pFlash.ErrorCode = 0x000000A0".is anybody have idea what problem is here i try example code too. I am totally beginner to stm3...

Ali110 by Associate II
  • 2530 Views
  • 2 replies
  • 0 kudos

STM32G431

I USED 6 PCS TIMER IN ENCODER MODE NEED ON SOFTWARE 64BIT POSITION I USED CHECK DIR AND SR BIT FOR TRAKING BOUT SOME TIME CHANGE DIR FAST AND I MAKE MISTAKE AROUND 65535HOPE ANY ONE CAN HELP HOW TO RESOLVED void tasktim2(void){ uint16_t b2; if ((TIM2...

Help needed, Flashing a FYSETC S6 V2.1 Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...

I'm looking for help, because I can not flash the FYSETC S6 V2.1, when trying to do so I get the error mesage. Technically very limited with Arduino, SMT32cubeprogrammer and FYSETC . My project is a OnStep telescope mount modification to remove DC ...

Pilleway by Associate
  • 2709 Views
  • 2 replies
  • 0 kudos

Resolved! To update DMA (array buffer) during runtime for changing duty cycle of TIMER 1 pwm complementary channels on STM32F103C8T6(bluePill).

My question is regarding HAL library in STM32F103C8T6(blue Pill) , I've just started using stm32 , I've good knowledge about arduino. I am trying to make sine PWM for a single phase inverter. For that i need channel1 of timer1 to generate complementa...

HJang.3 by Associate II
  • 3824 Views
  • 4 replies
  • 0 kudos

Resolved! Weird cycle behavior when running code from SRAM. 4 cycles per instruction instead of 1. What could be the cause?

Board: Nucleo-144Chip: STM32L4R5ZIT6PHey all!I have a curios problem when executing code from SRAM. My firmware lies in flash and occasionally jumps to a externally loaded binary in SRAM. As the cycle count of this binary is quite crucial, I used the...

LukasG by Associate II
  • 3450 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.