2022-09-09 2:27 AM
I'm working with the STM32F405 microcontroller and I want to receive packets over slave I2C using DMA, but I don't know on beforehand how big the next packet is. Is this not possible to achieve this without using a timer/polling mechanism that keeps investigating the received data and DMAx_Streamy->NDTR to determine when the reception is finished? I was thinking that I could use the stop condition interrupt from the I2C-peripheral, but it doesn't seem to work in conjunction with DMA. Does anybody know of a solution?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.