STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G030C8T6 readout protection doesn't work

I tried to set readout protection via ST-LINK CLI - it's enabled and disabled correctly, but after RDP=0 I can't erase/write chip - I've got an error on write operation. Tested on 2 boards and both boards have same behavior. e:\STM32 projects>"%PROGR...

NiTr0man by Associate III
  • 1081 Views
  • 5 replies
  • 2 kudos

Resolved! STM32H747-DISCO Core-Lock Problem

Hello,I’m using the STM32H747. When I set the RCC power source to RCC → Power parameters → Supply source = LDO, the core locks up; if I select SMPS, there’s no issue.When I set CM7 to its maximum clock frequency (480 MHz) and CM4 to 240 MHz, the tool...

CKILI.2 by Associate II
  • 1803 Views
  • 3 replies
  • 0 kudos

STM32L562 UART Data Rx packet loss

Hi,I am using USART4 in STM32L562E-DK eval board. with given configuration. In which I am able to transmit the data correctly on TX based on which UART slave device is sending back the 4 bytes ACK and 16 bytes RESPONSE.Using following codevoid HAL_UA...

414D414E_0-1757398146959.png
414D414E by Associate
  • 1173 Views
  • 5 replies
  • 2 kudos

i2s clock issue in stm32h723zg

hello, i hope you are doing good. i am facing an issue in configuring i2s in dev board nucleo-h723zissue i am facing is no clock at i2s2-sck pin.i tries all other i2s port also. i checked clock through logic analyzer .here is my clock configuration: ...

sajidehsan194_0-1757422544161.png sajidehsan194_1-1757422574730.png sajidehsan194_2-1757422636993.png

Resolved! STM32H743VIT6 ADC didn't run

Dear all!i'm handle graduation thesis project: " design driver for PMSM using STM32 base external mode with Matlab simulink"i design hardware as PDF file, all block working without ADC, i try to set up by STM32cubeMX 6.14 but it still can't run, so c...

Bootloader for STM32F746 for firmware and QSPI

Apparently I can not easily update my application firmware for stm32F746 toughGFX app with just one Bin file. I have written a bootloader for an SD card. It loads firmware at 0x08040000. I am not sure I understand everything that is going on here, so...

FJB2069 by Senior
  • 584 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F411 Blackpill + eMMC (Raspikey) + FatFS

Hi,I have a STM32F411CEU6 Blackpill that I'm wanting to interface to an eMMC (Raspikey to be exact via SD/MMC reader) with FATFS. I have confirmed that the connections with the SD/MMC reader are fine with a read/write test to an SD card in a differen...

chasej by Associate II
  • 1067 Views
  • 2 replies
  • 2 kudos

Resolved! STM32F303RET Clock Issue

I have a design that I have used in the past but a latest build I am having trouble with the system clock. I am using 8mhz crystal, IOC file HSE is setup to use the crystal. I cannot get the processor to run above 16 Mhz. I have older projects that u...

bradbas by Associate II
  • 1076 Views
  • 9 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.