STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC readings 'sticking' anomaly

I'm using the STM32H7B3.ADC configuration: Sample time : ~2usLL_ADC_SAMPLINGTIME_64CYCLES_5  Calibrations: HAL_ADCEx_LinearCalibration_FactorLoad(adc2)HAL_ADCEx_Calibration_Start(adc2, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED)Observations:The ADC counts se...

Sahiel_1-1753879721438.png Sahiel_2-1753881148542.png Sahiel_4-1753882434410.png
Sahiel by Associate II
  • 1541 Views
  • 12 replies
  • 3 kudos

what is the address on register A16

Post edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code #define FMC_BANK1_BASE ((uint32_t)0x60000000) ...

MNapi by Senior III
  • 374 Views
  • 0 replies
  • 0 kudos

STM32U375RGT6Q - UART function

Hi,Will PC0 PC1 LPUART functions in normal operation? I have to use this LPUART in normal operation of MCU, not in power saving mode.Is there any limitation on this like speed, baud rate etc. Regards,Anurag    

ADC Fluctuation

Hello,I have a ADC clock running at 96MHz prescaler divided by 10, 12bit, Sampling time 47.5 Cycles. I am just trying to sample this DC volgtages.  I have a battery that has around 20Volts, and I am stepping this voltage down using the voltage divide...

ytshin0877_4-1758084688725.png ytshin0877_0-1758083861526.png ytshin0877_3-1758084135450.png

Resolved! STM32H725VGH6 / Direct SMPS Supply / VLXSMPS Connection

Hi,We are using the STM32H725VGH6 MCU and are plannign to use the internal SMPS for VCORE.With regards to the connections required for the VLXSMPS pin, I would just like to confirm that a 220pF capacitor is required on this pin in the "Direct SMPS Su...

Figure3.png Table2.png Figure2.png
SammExa by Associate
  • 5196 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.