STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 ADC calibration, I don't understand

Hi all,I am experimenting with H7 ADC (after having tried the G4 ADC).I see in the HAL that the calibration, HAL_ADCEx_Calibration_Start(), for H7 MCU wants a parameter more than G4. One should specify ADC_CALIB_OFFSET or ADC_CALIB_OFFSET_LINEARITY.I...

linuxfan by Associate II
  • 4364 Views
  • 8 replies
  • 4 kudos

Resolved! STM32F401RBTx goes hard fault when clock speed is high

I saw a strange behavior when using STM32F401RBTx, to show you I added only 1 output as LED and  toggled it.  I have just that much code. I tried with 16 MHz, 48 MHz, 64 MHz, 84 MHz. It went hard fault when speed is 64 MHz or 84 MHz.    This is th...

alig_ones_0-1758196919434.png alig_ones_1-1758196967793.png alig_ones_2-1758197260671.png alig_ones_3-1758198391854.png

Resolved! The analog ground of STM32G473CBUx

Hi ST expertI'm ready to use STM32G473CBUx now. According to the datasheet, the STM32G473CBUx does not have an analog ground VSSA, only a ground VSS. I have questions:1. The analog input of the internal ADC/DAC is referenced to the chip's VSS, or has...

licunxu_0-1758162740290.png
licunxu by Associate II
  • 955 Views
  • 3 replies
  • 4 kudos

Resolved! HAL_UART_RxCpltCallback never triggers

I am implementing a system with two STM32H753 microcontrollers. MCU1 reads ADC data and sends it over UART to MCU2 using UART DMA on ADC conversion. MCU2 reads data from UART via DMA and is supposed to do some filtering (among other things) to the re...

Resolved! Cannot program STM32H750IBX, connection time out

Hello, We're working on a custom board for the STM32H750IBX. Our boards arrived. The first time, the chip was installed poorly and shorted out. We assembled a new board at the SMT factory with the new chip, but we still can't connect to the chip to p...

stm32h750ibx.PNG all on.png
ktak by Associate
  • 773 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.