STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Does STM32H7R7 LTDC support DE mode only?

Hi, I am evaluating the STM32H7R7Z8J6, intended to working with a TFT-LCD which is working in parallel RGB interface with DE mode only. The HSYNC and VSYNC signals are not connected. Both AN4861 (Introduction to LCD-TFT display controller (LTDC) on S...

Leo2Ruan by Associate III
  • 659 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 I2S master receive clock problem

Hi everyone,I am working on an STM32H7A3ZI and I'm trying to to exchange audio data with an SGTL5000 audio codec. Because i want to both send and receive data from the codec i configured the I2S peripheral on the STM32 to Full-Duplex Master mode in C...

QSPI Memory Read Write verification

Hi all! AGENDA: Need to verify the external QSPI flash (AT25Q128A) all sectors Write, Read and Comparing with STM32L496ZG-P using driver code. APPROACH: For write, I am have created a buffer which comprises of page size of 256, and I am using two "fo...

Abhiram_12_0-1758122487919.png Abhiram_12_1-1758122640047.png

Resolved! System Bootloader and Retaining the Last GPIO State

I have a problem I can't solve.In a previous project, I used an STM32L4A6 and set the PC8 and PC9 lines high before entering the system bootloader. After starting the system bootloader, these lines remained high. They were used to maintain power to t...

SKape by Associate II
  • 1074 Views
  • 4 replies
  • 1 kudos

Resolved! Built-in DFU bootloader and bAlternateSetting

Apologies if this is the wrong group for this query. I have implemented a library from scratch which performs the host side of a DFU upgrade (avoids the dependencies in CubeProgrammer_API.dll, for which I could not find source). The code works just f...

Boot problem with STM32N6

I am having trouble connecting to the STM32N6 with SWD.I have implemented a design using the STM32N645X0H3Q (though I have placed the STM32N647X0H3Q) using external VDDCORE. R110 is not mounted (to set VLXSMPS to NC).On startup I have VDDIO (3.3V) an...

edenraf by Associate II
  • 13462 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.