STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F303 setup ADC with all 4 ADCx.

Hello! I have a need to use ADC1, ADC2, ADC3 and ADC4 all at the same time, and preferably DMA on all of them too. I have not coded this yet, but I am mostly wondering if there are any pitfalls or things i should think about when doing this, so they ...

Resolved! Where can I find specs about DEMCR register on STM32H750XB ?

Hello,I cannot find more info about this register on RM or PM documents for STM32H750XB.I'm searching for register name. The register is about enabling debug features.Am I missing something or is this register described somewhere else (maybe for all ...

bully by Senior
  • 3573 Views
  • 4 replies
  • 0 kudos

Resolved! Unable to read ADC properly using STM32L073VZI6

Hello,I am using STM32L073VZI6 in a custom board, trying to read ADC values from a potentiometer connected to PA6. The microcontroller and the potentiometer are powered with 3.3 V.The issue is that I get 4095 when the voltage input is less than 2 V. ...

0693W00000WHjfLQAT.png 0693W00000WHjffQAD.png 0693W00000WHjfzQAD.png
JMart.28 by Associate II
  • 5687 Views
  • 7 replies
  • 0 kudos

Why not start touch with cubeprogrammer but only with stm32ide

HiI do have a program with touchgfx running on a stm32f746-disco.When program with stm32cibe IDE it starts up and running very fineBUT when i take the .elf file and program the board with the stm32cube programmer it do not start up touch ..what do yo...

hjh by Associate III
  • 2109 Views
  • 4 replies
  • 0 kudos

Resolved! Triggering ADC with Timer1 and Rpetition Counter

Hi There,I am currently working on ADC and Timer. I have 3 channels of ADC and using DMA. I want to trigger ADC at Timer1's update event. Also, I've set Timer's parameters to center aligned pwm, repetition counter to 1(with this I will trigger ADC at...

0693W00000WHsjqQAD.png

Why the number of pulses is less than expected when I am using One Pulse Mode and Repetition Counter (RCR) to generate adjustable PWM pulses with number and frequency?

I need to generate PWM signals with adjustable number and frequency to drive a step motor. I expect the frequency ranges from 50Hz to 200KHz and the pulses count ranges from 1 to 2k. I have tried 3 different ways including: using timer interrupt to c...

0693W00000WIBw5QAH.png 0693W00000WIBwAQAX.png
EMach.3 by Associate II
  • 3960 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.