STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to remove noise with touchgfx when using the QuadSPI

Hi. I made a project with stm32H743IIT6.i used ( touchgfx designer 4.20.0 ) + ( stm32cubeide 1.10.0 )and I saved my images on external flash (W25Q256) with QuadSPI and use SDRAM for touchgfx buffer.But I have a problem. when I display the image on LC...

davaba by Associate II
  • 2381 Views
  • 2 replies
  • 0 kudos

I want to do a pc waveform display of a four channel adc, it is a serial input pc and the sampling frequency is 1kSPS. What software should I use to develop, the sampling frequency is 2kSPS. I use node-red to find that the chart keeps crashing and can't g

I want to do a pc waveform display of a four channel adc, it is a serial input pc and the sampling frequency is 1kSPS. What software should I use to develop, the sampling frequency is 2kSPS. I use node-red to find that the chart keeps crashing and ca...

Lep by Senior
  • 736 Views
  • 0 replies
  • 0 kudos

Bug STM32F107RCTx SPI REMAPPED NOT WORK

STM32Cube FW_F1 V1.8.4Conditions: SPI1 or SPI3 remapped to PB3-5 pins. Problem: SPI not work.Solution: Enable Debug Serial Wire (PA13 PA14)SWJ function changes SWJ_CFG[2:0] bitsstm32f1xx_hal_msp.c line 81__HAL_AFIO_REMAP_SWJ_NOJTAG();do{ uint32_t tm...

vekli by Associate II
  • 1103 Views
  • 1 replies
  • 0 kudos

way to isolate stm32 chipset from NUCLEO board?

Hello, I would like to know the way to measure actual power consumption of stm32 chip on NUCLEO board, so if I disconnect:> LEDs> voltage regulators (supply 3.3vdc directly instead)am I able to get power consumption of stm32 chipset according to its ...

KPrem.2 by Associate
  • 1387 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.