STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

1.board-NUCLEO-H743ZI2 . we are dumping code into flash externally through USB .for that we are making boot0 pin high and low manually.is it possible to make boot0 pin high and low in software. I don't have access to change boot0 pin in MX.

we are not able to change boot0 pin in MX configuration. for other input output pins we are able to change the configuration but not for boot0 pin.Thanks in advance.

SChan.23 by Associate
  • 1869 Views
  • 3 replies
  • 0 kudos

FDCAN between two STM32H747 MCU boards

I would be interested in implementing a FDCAN communication between two STM32H747 MCU boards. I have implemented communication on a single board in External LoopBack mode. However, I am having problems understanding how to connect the two boards. Do ...

FVist.1 by Associate
  • 663 Views
  • 0 replies
  • 0 kudos

Keyboard scanner library sought

I'm in search for a library of routines that allow for scanning keyboard matrices with or without diodes in various configurations. I've heard it exists for Arduiono but I'm pretty sure there is such for the STM32 series too (my target is an STM32F10...

Controlling a Nucleo-L476RG Board Wirelessly

I am starting a DSP class project that will be auto-adjusting blinds using the Nucleo-L476RG board. To start off, I am wondering how it is possible to control the Nucleo board wirelessly with an android phone. I am aiming to control a stepper motor ...

JEscu.2 by Associate II
  • 1744 Views
  • 1 replies
  • 0 kudos

CAN Initialization failure then success

Hello,I have an interesting situation. When I start my app on the F303RE Nucleo I initialize all the peripherals. When CAN is initialized it returns a HAL_TIMEOUT error. If I call the same initialization code a second time it initialized correctly...

DPeki.1 by Associate II
  • 3616 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.