2022-11-14 3:43 AM
Hi Team,
Need the RTC Code base with LSE as clock source in wake-up counter mode and needs to get the interrupt at every 1sec rate.
We have some queries regarding the LSI Clock source which is in example project.
Regards,
Srinivas.V
2022-11-14 4:38 AM
What do you think of the suggestions made by @KDJEM.1 and @Community member in your previous, very similar question?
The need for calibration depends on your accuracy requirements. Calibration has often been discussed here in the community. You can use the LSE and either synchronise it with an external reference frequency (see reference manual), or use the so-called smooth calibration to correct the number of clock pulses entering the RTC, see e.g. here.
Regards
/Peter
2022-11-14 10:03 AM
Hi Peter,
Thanks for your reply. I do Understatnd the @KDJEM_1 Reply. In that example used the LSI Clock source and doing the auto calibration by using the another timer, that's where we need the more clarity, it that calibration is continuously required or just based on some condition. In the example code doing the calibration based on user key press.
That is the reason we are asking about LSE Clock source for RTC. How more accuracy as compared to LSI Clock. Just comparing the LSI and LSE Clock sources with respect to calibration Accuracy.
Regards,
Srinivas.V
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.