STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

High frequency DAC signal generation

Hi, i am working on signal wave generation on the STM32L053 Discovery kit. I'd like to see the maximum frequency of signal generation (a sinus with 100 samples using DMA). But the problem is : i cannot reach over ~20kHz, which is not even in the ultr...

0690X000008AH1fQAG.jpg
JFric by Associate II
  • 4830 Views
  • 6 replies
  • 0 kudos

STM32G031F6P UART TX DMA Problem.

Hi guys.I am using STM32G031F6P MCU and i want to use UART TX with DMA in slave mode. But it is not working. RS485 line is always busy. I am using RS485 transceiver (SN65HVD37DR). If i use normal (not DMA) transmit mode, it is working. Code and cubem...

0693W00000WITAJQA5.jpg 0693W00000WITATQA5.jpg 0693W00000WITCZQA5.jpg
ABURM by Senior
  • 1868 Views
  • 6 replies
  • 0 kudos

Reference pierce oscillator design available for STM32G0B1x?

I'm developing a new design with a STM32G0B1x uC. Therefore, I will use a 12MHz or 8Mhz external (HSE) crystal quartz from Abracon. I just read through the AN2867 and did some calculations. Now I'm at the point where I would need to measure the drive...

RHube.3 by Associate II
  • 2891 Views
  • 5 replies
  • 0 kudos

How to config FT231XS for STML451 on my board

I have a FT231XS on my board and a STML451. I would like to communicate over Uart to STM. So i need the FT231XS as USB to UART converter. My software works with NUCLEOL425RE, so when i send some strings over a Serial Port i can receive it immediately...

SMilo.3 by Associate II
  • 889 Views
  • 0 replies
  • 0 kudos

Resolved! 8bit in struct is allocated 32bit in memory

Hello,I am a newbie in struct.I have a struct declaration below.typedef struct __serial_data { uint8_t frameStart; uint32_t data; } serial_data;   serial_data mydata[25];but frameStart is allocated 32bit in memory and this causes trouble when sendi...

0693W00000WJH75QAH.png 0693W00000WJH7FQAX.png 0693W00000WJH7ZQAX.png

Call HAL_ADC_GetValue at any time.

I am using the ADC on an STM32 microcontroller.The ADC is operated in ContinuousConvMode.Can I start it with HAL_ADC_Start and query it at any time with HAL_ADC_GetValue?Or may HAL_ADC_GetValue only be used if it is ensured that the ADC is not curren...

mfrank9 by Associate III
  • 10110 Views
  • 2 replies
  • 1 kudos

Code won't run without pressing reset button

My code runs without issue when the STM Nucleo is connected to the laptop, but if I try to run it without connection to PC, I have to press the reset button before the code will run.I am using STM32CubeIDE and cannot find a solution relevant to that ...

IPrin.1 by Associate III
  • 9745 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.