STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No DAC output

It seems so easy, but I get no signal to the pin PA4. I use STM32f103VCT, any Idea ?int main(void){ /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all periphera...

jtozz.1 by Associate II
  • 5315 Views
  • 10 replies
  • 0 kudos

Support SPMI or I3C

HiI'm looking for STM32 board to support SPMI protocol or I3C.Is there any board that supports such a function?Thanks.

TKim.4 by Associate II
  • 1989 Views
  • 2 replies
  • 0 kudos

Resolved! Dropouts in ADC capture on STM32H743

If I connect a constant rising signal at the ADC input, I observe significant fluctuations at certain ADC values. These fluctuations always appear at the same ADC values. The affected values have the following format XX500, e.g. 18500, 19500, 20500 e...

ANovi.7 by Associate II
  • 17577 Views
  • 22 replies
  • 0 kudos

PWM input controlling PWM output

I have an interface that utilizes inverted PWM and I need a STM32F7 to receive and reply to messages from a controller. The controller sends 64 bit messages, the first 32 bits contains an address and if it matches with the address of the STM32F7, the...

Roth.Ian by Associate III
  • 1126 Views
  • 0 replies
  • 0 kudos

STM32 NUCLEO-F767ZI rs485

Hi i want to communicate between board with stm8 and board with stm32 the stm8 have rs485 communication bus does STM32 NUCLEO-F767ZI have build it in or i have to buy some extension?

uname.1 by Associate
  • 1526 Views
  • 1 replies
  • 0 kudos

Please can anyone show me a register that identifies the family "STM32F10x" of the MCU? I'm not interesting for a Unique device ID register "U_ID".

Hello,I would need a register that systematically identify the family type of the micro "STM32F103ZDT6".In the reference manual there is the Unique device ID register, but it gives a unique identifier to the chip, I would like an identifier that woul...

despo.1 by Associate
  • 2479 Views
  • 4 replies
  • 0 kudos

SDRAM Module Tester based on STM32F429

Hello everyone,I need to build a system to test a bunch of existing memory modules built around 512 Mbit SDRAM chips (4 chips each for total of 256 MBytes). The attached schematic shows the original design of the memory module and how it's connected ...

0693W00000WJDbGQAX.jpg
Zaher by Senior II
  • 1262 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.