When does FLASH lose data
在我的使用中,一些�?�数是在�?�片机(STM32F446ZET6)的闪存中�?置的,但在未知情况下�?�数丢失。在断电之�?,有断电和通电�?作。请问这是什么原因造�?的?解决方案是什么?
Ask questions, find answers, and share insights on STM32 products and their technical features.
在我的使用中,一些�?�数是在�?�片机(STM32F446ZET6)的闪存中�?置的,但在未知情况下�?�数丢失。在断电之�?,有断电和通电�?作。请问这是什么原因造�?的?解决方案是什么?
Often trip to Error_Handler from usb_device.c and usbd_conf.c.void Error_Handler(void){ /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CO...
Hello There,I'm looking to migrate from STM32F429ZIT6 to STM32H7A3ZIT6 for a TFT application.I have checked H7 will provide better performance on this.There is one more thing that comes to my mind that H7A3 has better specs than F429. Then why F429 p...
I'm new to the stm32MCU. I am using a Nucleo-U575zi-Q board. I am trying to read ADC values by setting the built-in DAC. I have check my DAC out and it is working fine. My ADC reading is giving me garbage values. I have set HAL_PWREx_EnableVddA() als...
Hi, I have a problem where I cannot debug my code bcs of this error. Anyone know how to solve these problem?btw im using the STM32H750VBT6x for MCU and ST-LINK V2
I am working with a NUCLEO_l452RE, temperature 25°C, 1.8V, and I am measuring current on JP6, so I tried to reproduce: I set up MSI@1Mhz, I got 280uA, much more than 100uA which I was expecting.Later with MSI@24Mhz, I got 3.24 mA, 135uA/MHz, closer t...
Hello,I have a question regarding several timers which are confiugred in PWM input mode (CCR1 is used to measure the PWM period and CCR2 is used to measure the PWM Width). So far when I plug a user signal on the evalution board, I can see the correct...
It is possible to use LPTIM to capture external pulse duration? I am using a SMT32L452 micro-controllerI think it is possible but I can't find hal for:Start lptim to capture external edgecallback functioncorrect setup on cube mx
We are porting code from a STM32L4P5, where we relocate the IRQ VEctor Table with memcpy(g_RamVectorTable, g_pfnVectors, sizeof(g_RamVectorTable)); __HAL_SYSCFG_REMAPMEMORY_SRAM(); // not implemented on STM32L5xxthat works fine, but as commented ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.