STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FLASH startup code does not branch to RAM

We have an STM32H750 ARM Cortex M7 processor in our product and are compiling C code using STM32CubeIDE. We want to have default code in FLASH that is able to run the default application by itself but which can also load an updated application to AXI...

Resolved! Configuration of OCTOSPI

1.in the manual "AN5050", What's the meaning of "memory type"? Does this mean that OCTO only supports these four types of memory chips? The flash I used is "IS25LP064A", Does the OCTOSPI support this flash?2.How to set the "DEVSIZE"? if the flash si...

0693W00000WK9HTQA1.jpg 0693W00000WK9HsQAL.jpg 0693W00000WK9I2QAL.jpg
rsun.11 by Associate II
  • 6172 Views
  • 9 replies
  • 0 kudos

No STLINK detected

Hello, everytime i try to run code in cubeide i get the message stlink not detected.I tried both on Linux and Windows and same problem appears.When i plug in my Nucleo F401RE the LED's do start blinking so i guess it is not a MCU problem. I also trie...

jl.11 by Associate
  • 1985 Views
  • 3 replies
  • 1 kudos

How to setup SPI mode 2?

I'd like to setup SPI mode 2 in my project with cpol=1 and cpha=0. But in SPI setup for cpha options are 1 or 2 edges. Which option do I have to select?

mladen by Associate II
  • 9135 Views
  • 6 replies
  • 0 kudos

Resolved! Why does UART4 RDR register not read anything? [SOLVED]

HelloI've been working for a few days with a BL475e IoT node that has a SMT32L475VGT6 microprocessor as standard.I am trying to communicate via UART with an Arduino UNO without satisfactory results. Below I share the code:I call from main() the follo...

SSeij.1 by Associate II
  • 2133 Views
  • 4 replies
  • 0 kudos

Nucleo H723 RTC under VBAT powering

Hello,I have set an RTC on a Nucleo H7 board and i I am powering it via VBAT pin when i switch off the VDD on the board. I have removed the 0Ohm connector from the SB52 and everything since working fine. When I reset the board for instance and I keep...

FCamp.1 by Associate III
  • 3150 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.