STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DMA LPUART work only once when power on

Hello everyone,I work on a project with STM32L072CBT6.I want to use a DMA RX on LPUART1, after reading differents ressources i have setup my LPUART and my DMA.I want to receive an interrupt from my DMA when transmit IDLE (end of transmit).My problem ...

0693W00000WL1NuQAL.png 0693W00000WL1OEQA1.png 0693W00000WL1OTQA1.png
MLam by Associate III
  • 2179 Views
  • 3 replies
  • 0 kudos

Need help in reading data from a pressure sensor

Hi!I'm new to embedded programming and I'm trying to write a minimal program using I2C to read data from a pressure sensor.I'm using the STM32F429 board and the Sen-16476 Sparkfun pressure sensor.I'm unsure about which pins I need to connect between ...

PReba.1 by Associate
  • 1732 Views
  • 2 replies
  • 0 kudos

Is STM32Lxx affected by PCN# MDG/22/13640?

Hello,Would you please double check are those low power types STM32Lxx affected by PCN# MDG/22/1364 as attached?In PCN only general purpose types STM32G070xx, STM32G071xx and STM32G081xx listed:In attachment “Public Product List�? low power types hav...

Joby by Associate
  • 2436 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L431VC - Can VREF+ be sequenced off of VDD/VDDA?

Hello - I am working on a safety critical application using the STM32L431VC that requires the VREF+ voltage rail to be powered off of a different voltage rail than the main VDD and VDDA rail. The VDD and VDDA voltage rails are being generated by a s...

0693W00000WKUiaQAH.png 0693W00000WKUizQAH.png

DAC not responding

I'm using the STM32H745I-DISCO board.I'm trying capture on the ADC and feed straight out on the DAC, triggered by a timer.The timer is working, and the ADC is getting data that looks sensible.I can see data reaching the DAC data register, but the out...

Hardfault Exception Debugging

The Hardfault Exception sometimes occurs during system operation.The register and stack values are as follows after the hardfault exception occurrence.The MSP 0x20003780 points to the stack area storing the register information(LR, PC etc) at the mom...

0693W00000WKbAkQAL.png 0693W00000WKbB4QAL.png 0693W00000WKbIjQAL.png 0693W00000WKbLJQA1.png
Kim.Andy by Associate III
  • 4088 Views
  • 5 replies
  • 0 kudos

hardware fault in stm STM32F733 . need recovery mech.

hi,I am getting hardware fault in stm and i found why it is happening .Now i want to rewrite the below function like clear the Int abd executing next instruction of stack.can i do like that .if possible is there any source code available for that.vo...

kchin.2 by Associate II
  • 2237 Views
  • 3 replies
  • 0 kudos

write internal flash with PVD interrupt

Hi everybody,I use a STM32L476RG. I'm trying to write 4 bytes in the flash memory on a PVD IT.I can write/read in the flash, it works.I've programmed my PVD on level 6 (2.9V) and BOR level is at 1.7V. I've used AN4718 to design a vbat system with a s...

fab04 by Senior
  • 1272 Views
  • 0 replies
  • 0 kudos

Resolved! What is the difference between parts “STM32F429ZGT6�? and "STM32F429ZGT6TR"?Can they be replaced each other pin to pin?Is the software compatible?

What is the difference between parts “STM32F429ZGT6�? and "STM32F429ZGT6TR"? W found from the datasheets,"*** = programmed parts,TR=tape and reel" .We think,“programmed parts�?should not be the same as "tape and reel".So the “TR�? really means?Can th...

ZJian.2 by Associate II
  • 2219 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.