STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDRAM : Some data not writting correctly

I am working on STM32H745BIT6 with W9812G6KH-6 SDRAM 16bit data bus. I have initialised the SDRAM and HAL driver seems to be returning HAL_OK so seems it is initialised properly.I write incremental data and read back. Observed some of the data not ge...

ATank.1 by Associate III
  • 2610 Views
  • 2 replies
  • 0 kudos

Need help with example code. I'm trying to do simultaneous ADC sampling on 3 analog inputs at 80KHz for 80 samples. Like to kickoff sampling on trigger from analog comparator. DMA samples to buffer and interrupt when buffer is full.

Thinking STM32G7474xx wound be a good fit but not sure. Need M4 CPU with FPU and low power modes. Like to have MCU in low power mode until buffer full. Any help would be greatly appreciated! I am new to ST MCU tools and not sure even where to begin....

MSamp.1 by Associate
  • 1253 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F030 Receiving UART Data Only Once

Hello,I'm trying to send data to STM32 from NodeMCU. My project is simply controlling WS2812B LEDs by using SPI from STM32 and receiving commands by using UART to STM32 from NodeMCU. LED's working fine by SPI but I can only receive data once at start...

salvi.a by Associate II
  • 1966 Views
  • 2 replies
  • 0 kudos

SPI write read is not done properly

Hello,I am working on STM32h7 controller. I configure the AD9106 DAC to SPI. When I tried to write read the configuration register some some registers are get read write and some not why these happening I check the register they are read write able ...

0693W00000WJOZpQAP.png
MDeva.1 by Associate II
  • 3814 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.