STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

When I program my device in debugging via JTAG/SWD with instances of low-power STOP mode within the code and disconnect Debugger, device never goes to sleep and get Ghost wake-up INTs. However, if I power cycle not pin reset device, every thing works.

Is there registers set by JTAG/SWD preventing sleep after programming.I also experience the same behavior after programming and reset within the STM32 ST-LINK Utility and not only within the IDE

UAnya.1 by Associate II
  • 2963 Views
  • 5 replies
  • 0 kudos

stm32g474 interrupt problem

Hi allI have a problem with interrupts on my STM32G474VEH6 based board. Timer 6 generates an interrupt every 1ms. Program crash at HAL_TIM_Base_Start_IT(&htim6);But after resetting the power of the board, the software starts working correctly.The sam...

RHert.1 by Associate II
  • 2994 Views
  • 5 replies
  • 0 kudos

Resolved! What is the letters -RBT6 -means in STM32G070RBT6 ?

Hey, I am working on STM32G070 development board.i downloaded from the orcad resources the scheme for the processor.however i can see it has additional letters and digits on the headercan someone explain me what are the meaninig of them?

0693W00000WLPKGQA5.png
YShko.1 by Associate II
  • 1646 Views
  • 2 replies
  • 0 kudos

i2c clock; how to config ?

in RM0008 Rev 21page 775Bits 5:0 FREQ[5:0]: Peripheral clock frequencythe description of the frequency divider is extremely unclear. there is no formula for where the input is, how it is divided, where the output is. what if I want to set strictly 50...

random number 0 to 255.

Hi! i want generate a random number into 0 to 255, i want use the random number for rutine neopixel color. i can use the rand() c function? the eand() function not generate number 0 to 255. Not need to be in ordem ascend or descend.

jdo by Associate II
  • 8133 Views
  • 6 replies
  • 0 kudos

Firmware source code *** boom for STEVAL-DPSLLCK1?

Hello, are the firmware source codes for STEVAL-DPSLLCK1 available?There is a diagram in the Data brief, but it does not contain more information about the main transformer, CT, etc., is there a complete boom of components?I didn't find it on the web...

Bazalt by Associate
  • 3039 Views
  • 5 replies
  • 0 kudos

Nor-flash external loader problem.

Hi,I followed the "How to create an external API loader MOOC" videos and after some struggle I managed to get it working for a board using the H7 with an Infineon S25FL127 memory.When I tried to do the same using a board with the G4 and with the same...

Asantos by Senior
  • 823 Views
  • 0 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.