STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U575 FMAC DMA wong amount of bytes

I have experimented with STM32U575Z using FMAC. I run the FMAC doing a convolution (sFmacConfig.Filter = FMAC_FUNC_CONVO_FIR) I run the FMAC in DMA mode. I registerd a HAL_FMAC_OUTPUT_DATA_READY Callback But it is never triggered. According to AN5593...

Basic timer questions STM32L476?

Hello all...Can someone give me direct answers below...(And please don't refer me to documentation as I have scoured thru it and not solved my questions)I would like some clarity as I have found no documentation to clarify the following:When using co...

SWenn.1 by Senior III
  • 1331 Views
  • 2 replies
  • 0 kudos

Why the interrupt is not triggered for RTC wakeup interrupt?

Hi,I am new to STM32 controller and I am using STM32L412RBT6. I was doing baremetal programming for RTC wakeup interrupt. But interrupt is not calling. Below mentioning my code. /* Enable Clock for Power interface.*/ RCC->APB1ENR1 |= (1U<<28); /*Disa...

SSaiy.1 by Associate III
  • 1191 Views
  • 1 replies
  • 0 kudos

Resolved! Why I2C communication fails between Ilps22qs and my nucleo?

I am working with STM32nucleoL476RG on a code able to establish an I2C communication between the pressure sensor Ilps22qs and my board. I am using the Qvar functionality, so I followed this pseudocode as reported on Qvar documentation:Write(0x10, 0x0...

Zenk91 by Associate II
  • 2648 Views
  • 4 replies
  • 0 kudos

Count External Pulses Using Timer

Hi All,First post :beaming_face_with_smiling_eyes: I want to count external pulses with a STM32F105 or STM32F405 using the HAL library. I want the external pulses to increment the timer counter. I want to avoid using interrupts. Instead, I want to re...

Resolved! CANBUS on F0 not able to receive.

I am working with the STM32F072CB device on a custom PCB. Working from this STM32 example.I just want to implement a basic loopback test. However i don't seem to receive any data.HAL_CAN_Init() is called succesfulHAL_CAN_Start() is called succesfulHA...

JWieb by Associate III
  • 1720 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.