STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to round division on STM32G0

I'm trying to implement an integer division with rounding. Obviously, by default integer division does floor and I was thinking I could use the remainder to determine if I should add 1 to my result.Processor cycles are at a premium in this solution (...

Konami by Senior II
  • 4994 Views
  • 7 replies
  • 0 kudos

Resolved! WARNING: CPU random generator seem to be failing, disable hardware random number generation WARNING: RDRND generated: 0xffffffff 0xffffffff 0xffffffffff 0xffffffffffffff

Hello community,since I updated the STM32 Cube IDE the following problem is displayed when entering the run or debug session.WARNING: CPU random generator seem to be failing, disable hardware random number generationWARNING: RDRND generated: 0xffffff...

TWI by Associate
  • 5484 Views
  • 2 replies
  • 0 kudos

I want to develop a C program on the STM32F303 board that uses the SPI interface where the microcontroller is the master and the L3GD20 gyroscope is the slave: I want to perform a transmission to ask the gyroscope to provide me with the x, y, z coordinate

Considering that the gyroscope's chip select is the PE3 pin, how should I do this? The program below doesn't work#include <stm32f30x.h>void GPIO_Config();void SPI_Config();uint8_t L3GD20_Read(uint8_t reg);void L3GD20_Write(uint8_t reg, uint8_t data);...

FPalo.1 by Associate II
  • 1734 Views
  • 2 replies
  • 0 kudos

STM32U5 ADC1 bulb sampling multiple channels

Hello,I am using ADC1 on STM32U5 to sample two channels periodically using the DMA and a TIM6 trigger. I am doing this in bulb mode since I would like for the ADC capacitor to charge for the entire duration.I had thought that the ADC would sample th...

F746 DMA from sdram to SPI

Is it possible to set transfer from sdram to SPI. I have set all necessary MPU regions and FMC is configured properly. When I use this with LTDC, it works fine.(not using standard DMA for that).But, when I try to send from 0xC0000000 to SPI, DMA1.str...

Gossamer by Associate II
  • 793 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.