STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Memory flash issue - read status register getting 0xff

Hi Experts,I'm working with the MCU "STM32F427VIT6" and the flash memory "GD25B16ETIGR" and I have a problem when I try to read the "read status register (05h)" I get 0xFF. However I know I have no problem on the SPI connection because I can read the...

TVela.1 by Associate III
  • 1946 Views
  • 1 replies
  • 0 kudos

HAL_SPI_ERROR_DMA

Hi, I am using stm32f769Ni evk for a project. Here I am interfacing stm32 with a wifi module using spi dma . The communication fails during reception with HAL_SPI_ERROR_DMA after  /* Enable the Tx DMA Stream/Channel */ if (HAL_OK != HAL_DMA_Start_IT(...

Rtomy.1 by Associate II
  • 4520 Views
  • 6 replies
  • 0 kudos

UDP Data Lost Issue

Hi,We're building our system based on STM32F407 with AZure Threadx + NetxDUO. One of the scenarios is as below:1) One 250 HZ task is responsible for sampling on 6 sensors connecting to 3 I2C.2) One UDP thread is receiving command from PC with 250HZ.3...

XLei.3 by Associate II
  • 875 Views
  • 0 replies
  • 0 kudos

Resolved! How to enable 100k cycles, instead of 10k cycles. [Resolved]

From RM0456-stm32u575585.... Flash section 7.3.8:"... up to256 Kbytes (32 pages) per bank feature an increased endurance of 100 kcycles, that can be used for data storage that usually needs more intensive cycling capability than codestorage. Any Flas...

SSaunders by Associate II
  • 8495 Views
  • 14 replies
  • 4 kudos

We connected STM32F051 to ASM330 over SPI . The communication works Chip select as a GPIO line the SPI is not able to correctly toggle the Chip select . There is a 10K ohm Pull-Up resistor on the Chip Select Line between STM and ASM . Is this correct ?

Hi ,We connected STM32F051 to ASM330 over SPI .The communication works Chip select as a GPIO line the SPI is not able to correctly toggle the Chip select . There is a 10K ohm Pull-Up resistor on the Chip Select Line between STM and ASM . Is this corr...

ck.1 by Associate III
  • 1934 Views
  • 2 replies
  • 0 kudos

How to run Bluetooth

I am going to start a project using BLE. And the board I am using is e B-U585I-IOT02A. There is already a Bluetooth module on this board. And I was thinking, is the Bluetooth is turned on by default, or do I have to activate it by myself ? My second...

TBarn.3 by Associate II
  • 1433 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.