Resolved! stm324x9i-eval example code packs
I have bought stm324x9i-eval in the past.I need a code pack of stm324x9i-eval examples.I'm using Keil uVision5 (MDK-ARM).I really need the stm32f MCU for training, so please help.
Ask questions, find answers, and share insights on STM32 products and their technical features.
I have bought stm324x9i-eval in the past.I need a code pack of stm324x9i-eval examples.I'm using Keil uVision5 (MDK-ARM).I really need the stm32f MCU for training, so please help.
Hi,I've been looking around in the documentation, and I can't find anywhere what the equivalent input circuit for the ADCs on the STM32F334 are. What is the input capacitance? What is the equivalent series resistance of the analog mux? What is the sa...
I am trying to print data over USART on the stm32g030c8t6. My code is as follows:/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main...
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) { if(GPIO_Pin == GPIO_PIN_10) { Switch10 = 1; HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, GPIO_PIN_SET); } if(GPIO_PIN == GPIO_PIN_11) { ...
//////////////////refresh pin HAL_GPIO_WritePin(GPIOA,GPIO_PIN_11,GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOA,GPIO_PIN_11,GPIO_PIN_RESET); HAL_Delay(10); HAL_GPIO_WritePin(GPIOA,GPIO_PIN_12,GPIO_PIN_SET); HAL_GPIO_WritePin(GPIOA,GPIO_PIN_12,GPIO_PIN_RESE...
Legacy:RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_BKPSRAM, ENABLE);RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE);Current: ?RCC_AHB1PeriphClockCmd(RCC_AHB1ENR_BKPSRAMEN_Msk, ENABLE);RCC_APB1PeriphClockCmd(RCC_APB1ENR_PWREN_Msk, ENABLE);
Hi, Now we want to use STM32F103 at -55C ambient temperature, MCUdata sheet say that it work at -40C as datasheet, storage temperature is -60C. My question is that,-If MCU is powered up at -55C, what will be different with>=-40C? Such as clock not st...
Using the IWDG within STM32L452 in its window mode.At some point the application needs to freeze the IWDG module functionality, or as a minimum make it work as in non-window mode.Is this possible? If yes, using which function?Note the I couldn't loca...
Hello, I am moving from TI DSPs to STM32 MCUs.I would like know if it is possible to configure SysTick timer to generate an interrupt with a period less than 1 ms, as I usually do on TI DSP projects.My doubt comes from UM2319, par 6.1.2:"SysTick time...
Is it possible to wake up from sleep when the UART receives one byte when I use cicular DMA?Or else I must catch every received byte using interrupt instead so it can wake up by interrupt.I'm using an STM32G030.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.