2023-02-22 6:19 PM
Hi,
Now we want to use STM32F103 at -55C ambient temperature, MCU
data sheet say that it work at -40C as datasheet, storage temperature is -60C.
My question is that,
-If MCU is powered up at -55C, what will be different with
>=-40C? Such as clock not stable,
-Do you have any -55C mcu as STM32F103 function for
recommendation?
Best Regards,
Kent
Solved! Go to Solution.
2023-02-23 12:31 AM
So far, no derivative of the STM32 is guaranteed to operate at a temperature lower than -40C. A statement about the behaviour at lower temperatures than the minimum operating temperature (most have -40C, a few -20C or -10C) can therefore not be made and one must assume that in extreme cases the STM32s will not work at all.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2023-02-23 12:31 AM
So far, no derivative of the STM32 is guaranteed to operate at a temperature lower than -40C. A statement about the behaviour at lower temperatures than the minimum operating temperature (most have -40C, a few -20C or -10C) can therefore not be made and one must assume that in extreme cases the STM32s will not work at all.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2023-02-23 12:55 AM
-55° is ->
so look for military spec. , Maxim Integrated has this, maybe stm has also.
example from Ti : MSP430F2619SPM , -55°C ~ 150°C
https://www.digikey.de/en/products/detail/MSP430F2619SPM/296-28280-ND/2353501
but about 120 € per piece ! so you have to pay for your "extras" .... :)
did a search on digikey
found only 1 from STM : SPC58EG80E5QEC0X
https://www.digikey.de/en/products/detail/stmicroelectronics/SPC58EG80E5QEC0X/16588292
2023-02-23 3:33 PM
It is helpful. TKS~ Kent
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.