STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CANbus: Check if CAN message failed to send X number of times

Hello,I am working on a CANbus communication with a critical system component that, if it is NOT communicating, portions of the systems should be shut down. I am trying to come up with a way to determine if communication is lost, but I feel like the ...

KMew by Senior III
  • 1064 Views
  • 0 replies
  • 0 kudos

STM32G0B1RE FDCAN normal / external loopback issue

Hi everyone,I am currently experiencing some issues with the FDCAN interface; my setup consists of two nucleo boards (Nucleo-G0B1RE) which use FDCAN interface to communicate with each other. As transceivers I am using two ATA6563-click boards.The clo...

0693W00000aHcAbQAK.png 0693W00000aHcAqQAK.png 0693W00000aHcC3QAK.jpg 0693W00000aHcAmQAK.jpg
lr2 by Associate
  • 2002 Views
  • 0 replies
  • 1 kudos

Resolved! Cannot get OCTOSPI example for STM32U575ZI MCU to work

Hello everyone,I am currently trying to connect a APS51208N PSRAM to a STM32U575ZIT6 using the OCTOSPI interface. I followed the steps for the first example in application note AN5050 (chapter 5.2.5, number 1). However when I step through the program...

PKolo.1 by Associate II
  • 3631 Views
  • 2 replies
  • 0 kudos

Can STM32F4 work as FSMC slave?

Hi, I am working on a design where FSMC interface is used. However, I need STM32F4 device to act as a slave on FSMC bus. Is STM32F4 able to act as the FSMC slave? Thank you.

TOlew.1 by Associate
  • 1620 Views
  • 1 replies
  • 0 kudos

STM32 and sim900a tcp/ip

Hi, i'm using an stm32F446re to read modbus rtu buffer from plc using usart1. now i need to send this data to a server using the gprs module sim900a on uart4 via tcp/ip. Any help please???????????

0693W00000YAoQQQA1.png 0693W00000YAokjQAD.png
fchai.1 by Associate II
  • 1815 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.