STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART escape sequences? NUCLEO-U575ZI

Hello everybody! I want to implement a simple UART debug/diagnose tool for my application, using UART on NUCLEO-U575ZI -> Termite or whatever other PC terminal program. Could please someone help me with a link to a list of escape sequences that I ca...

Skfir by Senior
  • 2966 Views
  • 6 replies
  • 0 kudos

ADC DMA not updating all channels

I'm using an STM32L4S9 MCU and I'm having trouble getting all the channels to update after starting ​HAL_ADC_Start_DMA. I'm doing a regular 12 bit conversion on 5 channels, trigger by software, waiting for conversion completed in the adc call back ...

SWood.4 by Associate III
  • 1920 Views
  • 1 replies
  • 0 kudos

Resolved! Weird behavior at HAL_GPIO function. Why the microcontroller is unable to set some pins after execute HAL code assertion statement?

I was running and debugging a part of my application on a stm32F207zg microcontroller.Microcontroller is on a custom PCB that is in validation process.This part of application has to set or clear 16 gpios configured as output.If they are initialized ...

0693W00000aHqGxQAK.jpg 0693W00000aHqX0QAK.jpg
genisuvi by Associate III
  • 3366 Views
  • 3 replies
  • 0 kudos

Resolved! How to make a PWM of 13.9ns pulse width with HRTIM?

Hello ST community,I use a STM32F3348 DISCO board (STM32F334C8Tx MCU) and I would like to realize a PWM with a period of 4µs (250 000 Hz) and a pulse width of 13,9ns. I tried first with the TIM1 and then with the HRTIM but in both cases I can't reduc...

PMach.2 by Associate II
  • 1471 Views
  • 1 replies
  • 1 kudos

Optimizing ADC DMA transfert and IRQ latency

Hello,I have the following config:STM32H743- Core 400MHz- AXI/AHB 200MHz- ADC clocked by the PLL at 144MHz, then divided by 4 (async mode) => 36MHz- TIM15 trigering ADC conversionsADC1 in scan mode converting 2 channels in scan mode. Data sent to SRA...

tarzan by Associate II
  • 2354 Views
  • 2 replies
  • 0 kudos

Implementation of a STM32 in transparent mode to flash another UART-connected STM32. What UART configurations and timing should be setting to implement this feature in STM32 in transparent mode?

I have one Master STM32 connected over UART to a Linux MPU and also connected over another UART to a Slave STM32.My purpose is to set the Slave STM32 in bootloader and flash from the MPU the application in the Slave STM32, the Master STM32 is in the ...

vincent by Associate II
  • 1480 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.