2023-02-13 5:24 AM
After changing some properties, those are:
-"BOR_LEV" set up 1 (BOR Level 2 VBOR2 brownout threshold level 2)
-"RDP" set up CC (level 2 chip protection)
from "Option Bytes" segmentation in STM Cube Programmer(It was unintentional case and before this fault, I have no problem in coding my MCU), the MCU(STM32F7xx) can not be seen any STM program anymore. If I should give some information about schematic design,
-BOOT0 is pulled down
-nRST is pulled up and goes directly programmer GND pin
-PDR_ON is pull-up.
Now, actually I dont know anything about RDP & BOR_LEV of option bytes. How can be turned back the situation for me? Do you have any advice?
Solved! Go to Solution.
2023-03-01 6:40 PM
2023-02-13 6:50 AM
I forgot to say that
when there is no problem, the old properties are like this
Read Out Protection:
RDP : 0xAA (Level 0, no protection)
BOR Level:
BOR_LEV : 0x0 (BOR Level 0)
2023-02-13 1:36 PM
> "RDP" set up CC (level 2 chip protection)
Yep, this.
> Now, actually I dont know anything about RDP & BOR_LEV of option bytes
Now you know something about the RDP ; )
2023-02-13 4:55 PM
> How can be turned back the situation for me?
RDP level 2 is a one way ticket. Now you've got a good lesson of why one has to read the documentation, not just click the broken bloatware generator.
2023-02-13 6:28 PM
>>Do you have any advice?
Replace the chip and start over
Tread more carefully
2023-02-26 9:46 PM
Thanks for quick reply and advise. I change my chip and go on my project. Actually, I try to create an external flash bootloader to my customized PCB. During this, I try to create my own .stldr (from copy and change the extension of .elf that created by STMCube Ide with proper configuration). Custom PCB has STM32F769NI as MCU and MX25L512G45 as external flash memory. And my goal is that some configuration data must be loaded to external flash via STMCubeProgrammer. But STMCubeProgrammer can not see external flash of the custom PCB if there is no specified bootloader for custom PCB. I believe that I apply all steps in this video but STMCubeProgrammer can see the external memory but could not erase or write anything (when I try to load my hex file). All in all, my actual problem brings to me this issue and still I could not solve my problem.
video link: https://www.youtube.com/watch?v=XqCq0xtQmbI
2023-02-27 12:52 AM
Specify the pins the QSPI uses an External Loader might exist for your combination.
2023-02-28 10:49 PM
I hope there is a customized loader .stdlr file such that fits my design :D. Here is my quadspi interface pins configurations:
QUADSPI_CLK --> PB2
QUADSPI_BK1_NCS--> PB6
QUADSPI_BK1_IO0 --> PF8
QUADSPI_BK1_IO1 -->PF9
QUADSPI_BK1_IO2 -->PE2
QUADSPI_BK1_IO3 -->PD13
And, my external flash is MX25L512G45.
2023-02-28 11:07 PM
Got something close, will check when I get up tomorrow.
2023-03-01 6:40 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.