STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Power on reset (PORRST) not detected on STM32L471RGT6

Hi, I am trying to detect whether a reset event was caused by power on rather than any other reset such as a button reset or a software reset. I attempted to use  if (__HAL_RCC_GET_FLAG(RCC_FLAG_PORRST) != RESET)but the compiler reports that PORRST ...

rwils.1 by Associate III
  • 4658 Views
  • 7 replies
  • 1 kudos

Resolved! Do the G4 series contain a DMA on timer break feature?

The RM0440 ch. 28.3.18 rev7 mentions on page 1128:> An interrupt is generated if the BIE bit in the TIMx_DIER register is set. A DMA request can be sent if the BDE bit in the TIMx_DIER register is set.Unfortunately, the DIER register does not contain...

Loebl by Associate II
  • 1957 Views
  • 2 replies
  • 1 kudos

Where single stepping with STM32H7 code works?

Some ARM/STM32H7 CPUs have a problem with single stepping through code. Which CPUs didn't have this problem? I have planned to use STM32H750 because it is now somewhat available, but I could swap.

LMI2 by Lead
  • 2059 Views
  • 3 replies
  • 0 kudos
SGhos.6 by Associate II
  • 2113 Views
  • 4 replies
  • 0 kudos

Resolved! CubeIDE --- How to change .ioc file to update another file??

Good morning.....I have a CubeIDE prj with .ioc and main. All compiles fine. I have created a second file with a main function (gfsk.c). I have excluded the original main.c for build. I would like to know when I go back into the .ioc to make a sm...

SWenn.1 by Senior III
  • 3136 Views
  • 2 replies
  • 0 kudos

Stm32f103c8t6 RTC Crystal Choice

Hi, I'm trying to do embedded 103c8t6, and I'm having some trouble with selecting the right crystal.Here is my Schematic. I'm using ABS07-32.768khz with 12.5pF load Capacitances and the equivalent series resistance is 70kR. I took Cstray as 5pF that'...

0693W00000aIpbIQAS.png 0693W00000aIpcuQAC.png
CArda.1 by Associate
  • 3580 Views
  • 2 replies
  • 0 kudos

Resolved! Older STM32H743ZI MCU Nucleo board was updated to V3.J10.M1 firmware version. While The board can be flashed, it isn't possible to debug or erase chip memory. Is there a way to roll back the update?

After running into some issues during an OS migration, I ran a firmware update on a nucelo_h743zi board using the stLink utility. After this I ran into many issues with flashing and debugging. While I can flash the board with openocd v11, it has some...

GToml.1 by Associate
  • 2317 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.