2023-03-13 11:03 AM
I have tested all 3v connections going into the st-link chip, but the bi-color led is not blinking when it is connected via USB. Please help.
2023-03-13 11:24 AM
Has it got firmware on it, and is it running?
2023-03-13 11:39 AM
No after assembling the pcb, I am unable to make any connection so far.
2023-03-13 11:44 AM
So you'll either need to use the System Loader, or another JTAG/SWD pod to get the firmware onto the STM32F1 chip.
The connectivity modes of the System Loader are described in app note AN2606
Then you'd need an actual firmware.
2023-03-13 11:55 AM
Thank you so much for your help.
So, I need to put a program to the STM32F103CBT6TR chip to act as an st-link for my stm32f4vgt6 chip, is that correct?
If so, then I need to generate a set of SWDIO, SWCLK, GND, and 3.3V to feed into STM32F103CBT6TR chip via another already programmed st-link v2.
Did I understand correctly?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.